×
Siemens Industry Online Support
Siemens AG
Type bericht: Productmededeling ID van bericht: 109793123, Datum bericht: 02/12/2021
(1)
Beoordelen

Delivery release PM-LOGON V1.8

  • Bericht
  • Heeft betrekking op product(en)
With immediate effect, PM-LOGON V1.8 is available. PM-LOGON V1.8 is a direct replacement for the predecessor version PM-LOGON V1.7 as a stand-alone and full version. The standard delivery of PM-LOGON V1.7 ends with the availability of PM-LOGON V1.8.

1. What's new?

Compared to PM-LOGON V1.7, PM-LOGON V1.8 features the following changes:

    • Additional logon providers: 
      • Windows Credential Provider for logon to Windows
      • Mobile Login for logon of a user to WinCC by using a mobile device (Android)
    • The PM-LOGON Runtime may now also be started as a system service 
    • Additional security features: 
      • Support of customer-specific keys for the encryption of the login data
      • Communication between PM-LOGON Runtimes based on HTTPS 
      • Certificate management in PM-LOGON Runtime
    • Release of additional SCADA System versions: 
      • SIMATIC WinCC V7.5 SP2
    • Support of additional card readers : 
      • Admitto-C TCP/IP reader

       

2. Delivery release information

  • With the delivery release of PM-LOGON V1.8 all PM-LOGON packages will be converted to V1.8. The licenses of PM-LOGON V1.x remain valid for PM-LOGON V1.8.
  • The order numbers remain unchanged for PM-LOGON V1.8 compared to PM-LOGON V1.7.


3. Supported operating systems and software requirments

3.1. Operating systems

With PM-LOGON V1.8 the following Microsoft operating systems are supported:

  • Windows 7 Professional, Enterprise, Ultimate 32-Bit / 64-Bit
  • Windows 8.1 Professional, Enterprise 32-/64-Bit
  • Windows 10 (64-Bit) Professional, Enterprise
  • Windows Server 2008 R2 (64-Bit)
  • Windows Server 2012 R2 (64-Bit)
  • Windows Server 2016 (64-Bit)
  • Windows Server 2019 (64-Bit)

3.2 Process communication / Base system:

With PM-LOGON V1.8 the following SIMATIC HMI-/SCADA systems are supported:

  • SIMATIC WinCC V 7.2
  • SIMATIC WinCC V7.3, V7.3 SE
  • SIMATIC WinCC V7.4, V7.4 SP1
  • SIMATIC WinCC V7.5, V7.5 SP1, V7.5 SP2
  • SIMATIC WinCC Runtime Professional V13, V13 SP1
  • SIMATIC WinCC Runtime Professional V14, V14 SP1
  • SIMATIC WinCC Runtime Professional V15, V15.1 (Upd. 1 or newer)
  • SIMATIC WinCC Runtime Professional V16
  • SIMATIC WinCC Runtime Advanced V13, V13 SP1, V13 SP2
  • SIMATIC WinCC Runtime Advanced V14, V14 SP1
  • SIMATIC WinCC Runtime Advanced V15, V15.1 (Upd. 1 or newer)
  • SIMATIC WinCC Runtime Advanced V16
  • SIMATIC WinCC flexible 2008 SP3
  • SIMATIC Logon V1.5, V1,6
  • SIMATIC WinCC WebNavigator ab V7.3

An overview of the supported base systems can be found at the PM-compatibility lists 


3.3 Compatible panels:

The following SIMATIC Multi- and Comfort panels are supported by PM-LOGON V1.8: 

  • TP700
  • TP900
  • TP1200
  • TP1500
  • TP1900
  • TP2200 


3.4 Supported card readers

PM-LOGON V1.8 supports the following card readers:


 Manufacturer Model Remark
Siemens AGSIMATIC RF1040R
SIMATIC RF1060R
SIMATIC RF1070R
 
Peter Hengstler Datentechnik GmbH

Admitto-A-Series
Admitto-C-Series

TCP/IP and USB-CDC-Mode

Important:
To work together with PM-LOGON the reader must be configured with a special parameter set by the manufacturer depending on the type of transponder to be used. The parameter set has to be specified already during the ordering process. For the exact ordering data please contact the WinCC Competence Center Mannheim 
HID GlobalOmnikey 5x2x-Series
Generic PC/SC-reader PM-LOGON supports other reading devices that provide a PC/SC interface. For additional information and prerequisites please contact the WinCC Competence Center Mannheim 
Generic COM-Port reader PM-LOGON supports other reading devices that provide a serial interface. The reading device has to transmit actively the UID of the transponder. For additional information and prerequisites please contact the WinCC Competence Center Mannheim.
Teratron GmbHPC-LOC USB readerFor additional information and prerequisites please contact the WinCC Competence Center Mannheim.
Euchner GmbH & Co. KGEuchner EKS USB reader (EKS-A-IUX-G01-ST01) 
R. STAHL HMI Systems GmbHEX-card reader UB03This card reader is supported in the modes “active send” and “phg_crypt”


3.5 Virtualization

Productive operation in virtualized environments or RDP-Sessions is not generally supported; the compatibility depends amongst other prerequisites on the used card reader device. If you are planning to use PM-LOGON in a productive virtualized environment, please contact the WinCC Competence Center Mannheim.

Further details and current compatibility statements can be found in the   PM-LOGON_V1.8_ReleaseNotes.pdf (108,8 KB) as well as in the Siemens compatibility tool 


4. Ordering data

The ordering data can be found at PM-order numbers 


5. Support and trainings for PM-LOGON  

For all PM-LOGON related topics (including trainings) the WinCC Competence Center Mannheim will be available for your requests:

Siemens AG
WinCC Competence Center Mannheim
Dynamostr. 4
68165 Mannheim, Germany

Tel.: +49 621 1723 1010
E-Mail: WinCCAddon.Automation@siemens.com 


6. Additional information

Further information to PM-LOGON can be found in the following articles:

Nota's in verband met security
Ter bescherming van technische infrastructuur, systemen, machines en netwerken tegen digitale dreigingen is het noodzakelijk om een alomvattend 'IT Security' concept te implementeren (en continu te handhaven) dat overeenkomt met de huidige stand van de techniek. De producten en oplossingen van Siemens vormen slechts een klein deel van een dergelijk concept. Meer informatie over 'Cyber Security' vindt u op
https://www.siemens.com/cybersecurity#Ouraspiration.
Bericht beoordelen
geen beoordeling
Verzoeken en feedback
Wat wilt u doen?
Opmerking: de feedback heeft altijd betrekking op het actuele artikel/product. Uw bericht wordt naar de technische redacteurs van de Online Support gestuurd. We zullen binnen enkele dagen antwoorden als uw feedback dat vereist. Als we geen vragen meer hebben, zullen we geen antwoord meer sturen.