×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109797645, Entry date: 05/18/2021
(3)
Rate

Download and sales/delivery release SINEC NMS V1.0 SP2

  • Entry
  • Associated product(s)
The product SINEC NMS V1.0 SP2 has been released for sale and is available for download. Please scroll down to “5. Download” to get a free 21-day trial version.

1. Product description 

The Network Management System for digital enterprise 

SINEC NMS is the Network Management System scalable for network structures of various sizes, in an increasingly digital world. This system can be used to centrally monitor, diagnose, and configure industrial networks with tens of thousands of devices around the clock. SINEC NMS is therefore the first choice for network management, and it’s paving the way for the digital transformation of industry – in all sectors and regardless of network size. Thanks to its scalability, SINEC NMS grows in parallel as the network becomes larger and more complex.

 

SINEC NMS V1.0 SP2 contains the following essential new features in addition to numerous smaller enhancements, comparing to the previous version: 

  • SINEC NMS system backup and restore
    • Auto / scheduled backup for the entire SINEC NMS system
    • Restore of SINEC NMS system in case of failure
  • New device family support: SIMATIC RFID portfolio
    • Integration of SIMATIC RFID portfolio: RF600, RF360R and RF18xC are now supported
    • Central discovery, monitoring, firmware handling and config file handling and policy-based device commissioning via OPC UA or PROFINET
  • New device family support: RUGGEDCOM WIN portfolio
    • Full support of RUGGEDCOM WIN device family 
    • Central discovery, monitoring, firmware handling and config file handling, config file handling (backup, restore, view, edit, compare)
  • Improved certificate management
    • SINEC NMS certificate management can be mapped to external root certificate
    • Seamless integration into customers’ existing certificate infrastructure
    • Certificate UI on Control and on Operation
    • Import / export certificates and renewing expired certificates
  • Customizable dashboard
    • New innovated dashboard with more information at a glance
    • Interactive widgets can be customized by drag & drop
  • Other new features
    • System
      • Simplified Chinese UI language
      • Microsoft Hyper-V
      • System Backup / Restore
      • Add Operation moved to overlay
    • Role-Based-Access-Control (RBAC)
      • Preselected user role for enforcement
      • Role “Superadmin” renamed to “super admin”
      • User must change password when it was changed by 3rd person
      • Profile settings and password can be changed independent from each other
    • Policy enforcement
      • Update only as option for firmware upgrade
      • Retry for firmware download
      • Navigate from Device list / Topology to Configuration Cockpit
      • Interface conditions for “Redundancy Protocol”
      • Updated WLAN tasks
      • New country codes for WLAN
      • Local user credential management on ROS devices
      • Rule Names can be changed
    • Northbound Interface
      • Dynamic parameters like “contentonly” for inherent login
    • UX improvement
      • Copy content from UI
      • Grids will show total and filtered amount of rows
      • General approach for allowed characters

  

2. Ordering data 

DVD: Software and license delivered by DVD package

OSD: Software and license delivered by Online Software Delivery (email address of receiving person is required)

SUS: Software Update Service

Power Pack: Upgrade from SINEMA Server V13/V14 to SINEC NMS, delivered by DVD package

  

Product name

Order number

SINEC NMS 50 V1.0 DVD

SINEC NMS 50 V1.0 OSD

SINEC NMS 50 V1.0 SUS

SINEC NMS 50 Power Pack

6GK8781-1BA01-0AA0

6GK8781-1BA01-0AK0

6GK8781-1BA00-0AL0

6GK8781-5BA00-0AC0

SINEC NMS 100 V1.0 DVD

SINEC NMS 100 V1.0 OSD

SINEC NMS 100 V1.0 SUS

SINEC NMS 100 Power Pack

6GK8781-1DA01-0AA0

6GK8781-1DA01-0AK0

6GK8781-1DA00-0AL0

6GK8781-5DA00-0AC0

SINEC NMS 250 V1.0 DVD

SINEC NMS 250 V1.0 OSD

SINEC NMS 250 V1.0 SUS

SINEC NMS 250 Power Pack

6GK8781-1JA01-0AA0

6GK8781-1JA01-0AK0

6GK8781-1JA00-0AL0

6GK8781-5JA00-0AC0

SINEC NMS 500 V1.0 DVD

SINEC NMS 500 V1.0 OSD

SINEC NMS 500 V1.0 SUS

SINEC NMS 500 Power Pack

6GK8781-1TA01-0AA0

6GK8781-1TA01-0AK0

6GK8781-1TA00-0AL0

6GK8781-5TA00-0AC0

 Link to the Mall:

https://mall.industry.siemens.com/mall/en/en/Catalog/Products/10349601?tree=CatalogTree 

 

3. Intended use 

High standards for highest demands 

The demands on a modern NMS are enormous. In addition to maximum transparency, scalability and availability, efficient user administration with simultaneous data security is required – as is overall user-friendliness. The ISO (International Organization for Standardization) defines what an NMS can achieve today in its FCAPS model. SINEC NMS supports all five cornerstones laid down in the FCAPS model.

  • Fault managementRecognizing, logging and correcting faults
  • Configuration managementDetermining and managing all the components to be monitored
  • Accounting managementAnalysis of the network use
  • Performance ManagementCollect performance data and keep statistics
  • Security ManagementAuthenticate users and authorize access and use

 

More than FCAPS 

SINEC NMS goes beyond FCAPS and offers two essential system elements that specifically address the industrial network’s requirements and are completing the functionalities of our NMS. 

  • Northbound Interface: This interface enables network and diagnostic data to be forwarded to different systems and applications, e.g., HMI and SCADA systems, via OPC UA.
  • System Administration: SINEC NMS is divided into a central control level and several distributed operational levels. This scalability feature allows it to grow along with the network as it becomes larger and more complex.

 

Efficient network management with a structured approach. 

  • Time savings: Configuration using SINEC NMS is policy-based, so it can be applied generically to multiple devices to save time.
  • Flexible scalability: The scalability feature of SINEC NMS allows it to grow along with the network as it becomes larger and more complex.
  • Security: With SINEC NMS, you meet the security requirements according to the IEC 62443.
  • Easy data handling: SINEC NMS ensures forwarding of network information for continued processing in other systems and applications, e.g., via OPC UA. 

 

4. Additional information 

Notes on installation/migration:

In addition to a new installation, the migration from previous versions of SINEC NMS to SINEC NMS V1.0 SP2 is also supported. 

When updating the SINEC NMS installations for Control and Operations to a higher SINEC NMS version, the existing data are retained for the most part.

 

UMC

The UMC version contained in the SINEC NMS V1.0 SP2 installation package has been updated to SINEC NMS V1.0 SP2. If you want to use this UMC version in SINEC NMS V1.0 SP2, you need to install and set up UMC again. An existing UMC installation from previous SINEC NMS versions will be automatically uninstalled from SINEC NMS V1.0 SP2 before the new UMC version is installed. Other UMC installations must be uninstalled manually beforehand. The UMC user groups contained in previous SINEC NMS versions are transferred to SINEC NMS V1.0 SP2 during migration. UMC data are not transferred when the new UMC version is installed. UMC needs to be licensed separately. Please refer to the user manual for more information.

 

Refer to the installation and usage notes in the following file: 

English:  Registrierung notwendig  ReadMe.html (121,6 KB) 

German:  Registrierung notwendig  LiesMich.html (113,7 KB) 

Simplified Chinese:  Registrierung notwendig  Zh_ReadMe.html (221,6 KB) 

 

 

5. Download 

Third-party software – license conditions and copyright notes

You can find the copyright information for third-party software contained in this product, particularly open-source software, as well as applicable license conditions of such third-party software in the OSS_SINEC-NMS_99.pdf file.

Special note for resellers

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

  OSS_SINEC-NMS_99.pdf (12,8 MB) 

 

 

SINEC NMS V1.0 SP2:

A 21-day trial license is automatically activated if no other license type has been found by the Automation License Manager when SINEC NMS starts the first time. The following restrictions apply as compared to the full version:

  • Max. 3 devices in the "Managed" management status, max. 500 devices with the "Monitored" management status.
  • Causes for results of validation reports are not displayed, and it is also not possible to generate pictures of the topology display.

 


 Registrierung notwendig  SINECNMS_V1.0_SP2.exe (2,8 GB)

Hash:  Registrierung notwendig  SINECNMS_V1.0_SP2.txt (1 KB)

 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.