×
Siemens Industry Online Support
Siemens AG
寄稿のタイプ: ダウンロード 寄稿のID: 109798579, 寄稿の日付: 06/09/2021
(0)
評価する

Firmware update for ET 200M IM153-2 HF OUTDOOR

  • 寄稿
  • 製品に関係する
Firmware update for ET200M IM153-2 HF OUTDOOR

Description

When firmware is updated, it must always be updated to the latest version available for the product with the relevant article number. The previous versions of the firmware are only intended as a backup to enable you to downgrade to the original version.

The latest version of firmware in each case is valid for all revision levels of this article number.

1. Online firmware update via HW-Config:

  1. Download the desired firmware file
  2. Extract the files
  3. Select the corresponding ET200M station in HW Config
  4. Program the firmware by selecting in the program menu: "PLC > Update firmware"
  5. Select the directory with the firmware file in the directory and start the firmware download

The download process is not visible on the IM153-2. After successful download, the new firmware can be started automatically or with power off/on.

2. Online firmware update via SIMATIC Manager:

  1. Download the desired firmware file.
  2. Extract the files.
  3. Connect the programming device with the stream to which the ET200M station is connected
  4. In SIMATIC Manager, open the 'Accessible devices' view and select the station address
  5. Program the firmware by selecting in the program menu: "PLC > Update firmware"
  6. Select the directory with the firmware file in the directory and start the firmware download

The download process is not visible on the IM153-2. After successful download, the new firmware can be started automatically or with power off/on.

Update V6.1.6

Optimizations and additional features:

  • Optimization of time stamping when operated with S7-400H
  • Optimization of consistency check of module memory
  • Optimization of operation mode Y-Link
  • Feature Servicedata implemented
  • Optimization of diagnostics behaviour
  • Remanent storage of diagnostic data on the IM
  • Implementation of extended diagnostic data and read service data via STEP 7 Classic, HSP0246 V3.2
  • Optimization of redundancy switchover
  • Optimization of acyclic functions, such as FW-Update, S7-Online, etc.

The firmware V6.1.6 is provided at no cost for download and can be transferred to the device using standard means. The system can be upgraded with costs at the factory.

Übersicht der Artikelnummer und aktuellen Firmware-Versionen der ET 200M IM153-2 HF OUTDOOR:

Article numberFirmware
version
Download
 6ES7153-2BA70-0XB0V6.1.6

 Registrierung notwendig  6ES7153-2BA70-0XB0_FW_V616 (363,8 KB)(SHA-256)







セキュリティ情報
技術的なインフラストラクチャー、システム、機械とネットワークをサイバー脅威から守るために、現在の技術の状態に応じた全体的なITセキュリティーコンセプトを実装すること(そして持続的に維持すること)が必要です。シーメンスの製品とソリューションはそのようなコンセプトの1つの要素だけを形成します。サイバーセキュリティーについての詳細は以下をご覧ください:
https://www.siemens.com/cybersecurity#Ouraspiration.
寄稿を評価する
評価なし
リクエストとフィードバック
何をしたいですか?
注: フィードバックは常に現在のエントリ / 製品に関連しています。メッセージは、オンラインサポートで作業しているテクニカルエディタに転送されます。フィードバックに応答が必要な場合は、数日以内に返信いたします。これ以上問題がない場合、ご連絡はいたしません。
統計に対するサポート
この機能によって、希望する数に基づく検索結果のIDが出力されます (format .txt)

Generate list
URL をコピーする
このページを新しいデザインで表示する
mySupport コックピット