×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109801209, Entry date: 09/16/2021
(2)
Rate

Integration of a SIMATIC ET 200SP HA in TIA Portal

  • Entry
  • Associated product(s)
The SIMATIC ET 200SP HA offers a flexible, scalable and fault-tolerant distributed I/O system. You will learn how to integrate the SIMATIC ET 200SP HA into automation systems in TIA Portal, how to implement a cross-channel and channel-specific signal configuration in SIMATIC TIA Portal, as well as how to replace I/O modules while in operation (Hot Swap).


The SIMATIC ET 200 product family has long been a corner stone for flexible, distributed solutions that can be customized for any automation task. The new concept of the SIMATIC ET 200SP HA combines this flexibility with highest system availability and an even smaller footprint. The new design allows up to a maximum of 56 I/O modules per station. An impressively high concentration of up to 32 channels on a module that is only 22.5 mm wide allows maximum space utilization in the
control cabinet.


The PROFINET communication standard is used for linking process signals to a superordinate controller, e.g. an S7-1500R/H.

The SIMATIC ET 200SP HA supports the following PROFINET functionalities:

  • simple S1 system connection
  • simple S2 system redundancy and
  • Media Redundancy Protocol (MRP)

This means that the SIMATIC ET 200SP HA can be linked both to standard as well as to fault-tolerant automation systems. Changes to the configuration during operation are supported if the corresponding prerequisites are met.





Through this application example you will learn step by step

  • how to configure the SIMATIC ET 200SP HA,
  • what diagnostic options TIA Portal offers,
  • how to replace an I/O module while in operation and while voltage is applied,
  • how to add and confifure an explosion-protected I/O module to your station while in operation and 
  • how to parametrize HART field devices with SIMATIC PDM.

Download

  Documentation ET 200SP HA in TIA (2,0 MB)


Further informationen

Application Example for integration of SIMATIC CFU in the TIA Portal

Functional overview of SIMATIC ET 200SP HA in SIMATIC PCS 7, SIMATIC PCS neo, SIMATIC STEP 7 and SIMATIC STEP 7 (TIA Portal)

Product note - SIMATIC ET 200SP HA Distributed I/O system


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.