×
Siemens Industry Online Support
Siemens AG
Entry type: Download, Entry ID: 114358, Entry date: 05/12/2017
(106)
Rate

Automation License Manager (ALM), AuthorsW and Authors handling programs and authorizing and licensing SIMATIC Industry Software

  • Entry
  • Associated product(s)
Here, we provide packed download files with the latest versions of these licensing programs for MS-DOS and Windows.

Description
Authorization of SIMATIC Industry Software requires a red or yellow authorization disk. This disk might include an older version of the Windows handling program AuthorsW or the handling program AUTHORS (MS-DOS) for transferring the authorization. Later software packages install the version V2.4.2 or V2.5.2 of AuthorsW on the hard disk and register it in the system. In this case there is no handling program on the authorization disk.

The new licensing procedure with license keys was introduced in 2003. These keys are supplied on the yellow license disks, on USB sticks or via downloads from the A&D Mall, or are already preinstalled on a Compact Flash Card. The license keys can only be handled with the Automation License Manager (ALM) handling program that is on the associated CD and which is automatically installed by default with the software. More information on license keys is available in Entry ID: 19100818.

Get in touch with Technical Support if your license key or authorization is defective. The Technical Support will support you to restore defective license keys and authorizations. Further informations you will find by entry id: 772175.
 

 No.Handling programs 
1Automation License Manager V5.3
The packed file "114358_ALM_V5_3_SP3_Upd3.zip" contains the installation software for ALM V5.3+SP3+Update3 and is enabled 

for the 32-bit operating systems below:

  • MS Windows XP SP2 or SP3
  • MS Windows Server 2008 with or without SP2
  • MS Windows 7 (32 Bit) with or without SP1
  • MS Windows 8.1
  • MS Windows 10

and for the 64-bit operating systems below:

  • MS Windows Server 2008 R2
  • MS Windows 7 (64 Bit) with or without SP1
  • MS Windows 8.1
  • MS Windows Server 2012
  • MS Windows 10


Security Note
The Automation License Manager version V5.3 onwards includes important security improvements. If you have version of ALM previous to V5.3, we recommend installing this update immediately. This update is compatible with all ALM V4.0 versions and higher. The above-mentioned operating systems are supported by the Automation License Manager in order of their product release.


Installation
Upgrading of the operating system is not supported. More information is available in the ALM readme file. Proceed as follows to install.

  1. Click the "114358_ALM_V5_3_SP3_Upd3.zip" link to open the packed file.
  2. Unpack the file in a separate directory on your hard disk.
  3. Close all the programs before starting the Setup.
  4. Start the "Setup.exe" in your directory.
  5. Follow the instructions of the installation program.


Note
A check is made automatically before the installation as to whether your operating system is compatible. Then the version of ALM relevant for your operating system is installed (32-bit or 64-bit). You can also start one of the lower-level installation programs in the "ALM32" or "ALM64" folder. Example:

  • for Windows 7 (32-bit) the "Setup.exe" in the "ALM32" folder
  • for Windows 7 (64-bit) the "Setup.exe" in the "ALM64" folder


 Registrierung notwendig  114358_ALM_V5_3_SP3_Upd3.zip (126,9 MB)

2Windows handling program AuthorsW V2.5.2
The packed file (AuthorsW252) contains the AuthorsW V2.5.2 installation software. After downloading, AuthorsW V2.5.2 is installed with an InstallShield Setup and employs the Registry.

AuthorsW252.zip ( 5339 KB ) 

3MS-DOS handling program AUTHORS V 4.5
The packed file (Authors45) contains AUTHORS V4.5 that can be used with the authorization disks listed below. The transfer must be made on disks that already contain AUTHORS V4.x, or on an authorization disk that contains AUTHORS from version V3.04 of 07.03.96 (for example, STEP 5 as from V6.6 or STEP 7 as from V2.0).

Authors45.zip ( 198 KB ) 


Authorization hotlines
 

  Telephone Link/E-mail
 Europe/Africa+49 (0) 911 895 7222Support Request 
 AmericaToll Free
+ 1 800-333-7421
Outside USA
+1 423-262-2522
Support Request 
 Asia/Australia+86 10 64 757575support.asia.automation@siemens.com 

Additional Keywords
License

 

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.