Entry type: Download, Entry ID: 114358, Entry date: 01/13/2015
(10)
Rate

Automation License Manager (ALM), AuthorsW and Authors handling programs and authorizing and licensing SIMATIC Industry Software

  • Entry
  • Associated product(s)

Description

Authorization hotlines
 

Telephone Fax Link/E-mail
Europe/Africa +49 (0) 911 895 7222 +49 (0) 911 895 7223

Support Request

America Toll Free
+ 1 800-333-7421
Outside USA
+1 423-262-2522
+1 678 297 8316 support.usa.automation@siemens.com
Asia/Australia +86 10 64 757575 +86 10 64 747474 support.asia.automation@siemens.com

Authorization of SIMATIC Industry Software requires a red or yellow authorization disk. This disk might include an older version of the Windows handling program AuthorsW or the handling program AUTHORS (MS-DOS) for transferring the authorization. Later software packages install the version V2.4.2 or V2.5.2 of AuthorsW on the hard disk and register it in the system. In this case there is no handling program on the authorization disk.

The new licensing procedure with license keys was introduced in 2003. These keys are supplied on the yellow license disks, on USB sticks or via downloads from the A&D Mall, or are already preinstalled on a Compact Flash Card. The license keys can only be handled with the Automation License Manager (ALM) handling program that is on the associated CD and which is automatically installed by default with the software. More information on license keys is available in Entry ID: 19100818.

Here, we provide packed download files with the latest versions of these licensing programs for MS-DOS and Windows.

A support form for submitting a service request can be called and filled in for AuthorsW and then sent to the Support office concerned if they cannot be reached by phone. Where: AuthSuppA=deutsch, AuthSuppB=english, AuthSuppC=francais, AuthSuppD=espanol, AuthSuppE=italiano. More information is available in Entry ID: 772175.
 

No. Handling programs
1 Automation License Manager V5.3
The packed file "ALM_V5_3_SP2_Upd2.zip" contains the installation software for ALM V5.3+SP2+Update2 and is enabled 

for the 32-bit operating systems below:

  • MS Windows XP SP2 or SP3
  • MS Windows Server 2003 SP1 or SP2 Standard Edition with or without R2
  • MS Windows Server 2008 with or without SP2
  • MS Windows 7 (32 Bit) with or without SP1
  • MS Windows 8 and 8.1

and for the 64-bit operating systems below:

  • MS Windows Server 2008 R2 with or without SP1
  • MS Windows 7 (64 Bit) with or without SP1
  • MS Windows 8 and 8.1
  • MS Windows Server 2012

Security Note
The Automation License Manager version V5.2 onwards includes important security improvements. If you have version of ALM previous to V5.2, we recommend installing this update immediately. This update is compatible with all ALM V4.0 versions and higher. The above-mentioned operating systems are supported by the Automation License Manager in order of their product release.

Installation
Upgrading of the operating system is not supported. More information is available in the ALM readme file. Proceed as follows to install.

  1. Click the "ALM_V5_3_SP2_Upd2.zip" link to open the packed file.
  2. Unpack the file in a separate directory on your hard disk.
  3. Close all the programs before starting the Setup.
  4. Start the "Setup.exe" in your directory.
  5. Follow the instructions of the installation program.

Note
A check is made automatically before the installation as to whether your operating system is compatible. Then the version of ALM relevant for your operating system is installed (32-bit or 64-bit). You can also start one of the lower-level installation programs in the "ALM32" or "ALM64" folder. Example:

  • for Windows 7 (32-bit) the "Setup.exe" in the "ALM32" folder
  • for Windows 7 (64-bit) the "Setup.exe" in the "ALM64" folder

ALM_V5_3_SP2_Upd2.zip ( 131694 KB )

2 Windows handling program AuthorsW V2.5.2
The packed file (AuthorsW252) contains the AuthorsW V2.5.2 installation software. After downloading, AuthorsW V2.5.2 is installed with an InstallShield Setup and employs the Registry.

AuthorsW252.zip ( 5339 KB )

3 MS-DOS handling program AUTHORS V 4.5
The packed file (Authors45) contains AUTHORS V4.5 that can be used with the authorization disks listed below. The transfer must be made on disks that already contain AUTHORS V4.x, or on an authorization disk that contains AUTHORS from version V3.04 of 07.03.96 (for example, STEP 5 as from V6.6 or STEP 7 as from V2.0).

Authors45.zip ( 198 KB )

Additional Keywords
License

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster