×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 11448268, Entry date: 05/17/2002
(0)
Rate

Driver for Norton Ghost

  • Entry
  • Associated product(s)

QUESTION:
Why, when booting with the boot floppy disk created by Norton Ghost, do I get the following error message?

  • Intel(R) PRO PCI Adapter  v3.38 (981117)
  • Copyright 1998, Intel Corporation.  All Rights Reserved.
  • E100BODI-DOS-1: The LSL is not loaded.

ANSWER:  
The Norton Ghost software is a DOS program for creating a hard disk image (hard disk copy). The Ghost network boot wizard also offers you the Intel driver "INTEL ETHER EXpress 10-100 PCI NDIS". Please select this driver to clear the above-mentioned error message. Please also check settings in the BIOS Setup:

  • Installed OS:            Other
  • Onboard Ethernet:   Enabled

Keywords:
Onboard Intel LAN adapter

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.