DriveMonitor Version V5.5 SP2 for SIMOVERT MASTERDRIVES, MICROMASTER and SIMOREG.
-
Entry
-
Associated product(s)
Description
The updated version V5.5 SP2 of the DriveMonitor commissioning tool for the device families SIMOVERT MASTERDRIVES, MICROMASTER 3, MICROMASTER 4 and SIMOREG is provided here. The Release V5.5 SP2 replaces all existing Releases V5.x and can be installed both as a stand-alone version and as an update for Drive ES Basic Version V5.1 SP1 (or later).
Hint
This version of DriveMonitor (incl. HF1) is part of Drive ES Basic Maintenance V5.6 (see 109749732).
The DriveMonitor 5.5 SP2 can be executed with the following operating systems
- MS Windows 2000 SP4
- Microsoft Windows XP Professional SP2 *) and SP3
- Microsoft Windows 2003 Server SP2
- Microsoft Windows VISTA Business SP1 *)
- Microsoft Windows VISTA Ultimate SP1 *)
- Microsoft Windows 2008 Server
- Microsoft Windows 7 Professional (32 / 64 Bit)
- Microsoft Windows 7 Ultimate (32 / 64 Bit)
- Microsoft Windows 8 (32 / 64 Bit) **)
- Microsoft Windows 8 Pro (32 / 64 Bit) **)
- Microsoft Windows 8.1 (32 / 64 Bit)
- Microsoft Windows 8.1 Pro (32 / 64 Bit)
- Microsoft Windows 10 (64 Bit)
- Microsoft Internet Explorer V6.0 (or later)
*) The functional scope has not been tested completely. You can use it on your own risk.
**) Strictly limited test scope, that means, you can only install it on your own risk, after acknowledging the relevant warning message.
Drive Monitor 5.5 SP2 functional changes / extensions
- Support of operating system Windows 8.1 (32 / 64 Bit)
- Installation problems with V5.5 SP1 in some environments
DriveMonitor V5.5 SP2
11769381_drivemonitor_v5_5_sp2.zip (466,2 MB)
HF1 for DriveMonitor V5.5 SP2
11769381_DriveMonitorV5.5_SP2_HF1.zip (8,4 MB)
This HF1 can only be installed if DriveMonitor V5.5 SP2 is present.
HF2 for DriveMonitor V5.5 SP2 (only for environments without MSXML V4.0 SPx)
DriveMonitor could have problems, if at newer operating system environments the MicroSoft-component MSXML V4.0 SPx is not available. This problems can be solved by the installation of the HF2:
11769381_DriveMonitorV5.5_SP2_HF2.zip (9,4 MB)
This HF2 can only be installed if DriveMonitor V5.5 SP2 is present.
- German
- Chinese
Entry belongs to product tree folder(s):
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 4 MICROMASTER 410
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 4 MICROMASTER 411 / COMBIMASTER 411
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 4 MICROMASTER 420
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 4 MICROMASTER 430
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 4 MICROMASTER 440
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 4 Accessories
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 3 Standard
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 3 Vector
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 3 Eco
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 3 Accessories
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters Archive MICROMASTER 4 MICROMASTER 410
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters Archive MICROMASTER 4 MICROMASTER 420
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters Archive MICROMASTER 4 MICROMASTER 430
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters Archive MICROMASTER 4 MICROMASTER 440
- Drive Technology Converters Low voltage converters SIMOVERT MASTERDRIVES Frequency Converters SIMOVERT MASTERDRIVES MC frequency converters
- Drive Technology Converters Low voltage converters SIMOVERT MASTERDRIVES Frequency Converters SIMOVERT MASTERDRIVES VC frequency converters < 200 kW
- Drive Technology Converters Low voltage converters SIMOVERT MASTERDRIVES Frequency Converters SIMOVERT MASTERDRIVES VC frequency converters SIMOVERT MASTERDRIVES VC > 200 kW
- Drive Technology Converters Low voltage converters SIMOVERT MASTERDRIVES Frequency Converters Active Front End (AFE)
- Drive Technology Selection and engineering tools DriveMonitor Commissioning Software
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry