×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 11886029, Entry date: 05/16/2018
(0)
Rate

Which I/O modules can be used in combination with SIMOTION?

  • Entry
  • Associated product(s)
Compatibility list of the I/O modules which can be used with SIMOTION.

When integrating I/O modules, you can use the range of I/O modules of SIMATIC and SINAMICS.

The I/O modules which have been released for SIMOTION are listed in the following compatibility matrix. If you want to integrate modules which are not listed in the compatibility matrix, please contact your local Siemens office.

The range of I/O modules which have been integrated is continuously expanded.

SIMATIC I/Os
SIMATIC_IO_Modules_for_SIMOTION.pdf (782.4 KB)

SINAMICS I/Os
SINAMICS_IO_Modules_for_SIMOTION.pdf (50.6 KB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.