×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 11965598, Entry date: 06/17/2002
(1)
Rate

New Document CDs for MICROMASTER 420 and MICROMASTER 440

  • Entry
  • Associated product(s)
...




There are new Document CDs for the MICROMASTER 420, V1.0x, and MICROMASTER 440, V2.0x, inverters.

The Operating Instructions and Parameter Lists have been revised and are now available in the following languages:

  • English
  • German
  • French
  • Spain
  • Italian

The CDs contain the following commissioning tools

  • Starter V2.0
  • DriveMonitor V5.1, SP1, HF2

Each MICROMASTER 420 and MICROMASTER 440 is delivered with the appropriate Document CD as standard.

The CDs can also be ordered separately at a price of 5 € each

Order Nos.:

  • MICROMASTER 420: 6SE6400-5AB00-1AP0
  • MICROMASTER 440: 6SE6400-5AD00-1AP0

Operating Instructions and Parameter List are also available in the Internet at: 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.