×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 12184419, Entry date: 07/05/2002
(0)
Rate

SIMATIC Box PC 840 Now Available with CD-R/RW/DVD Drive  

  • Entry
  • Associated product(s)
>


With immediate effect, the new optical drive option CD-R/RW/DVD can be ordered for the SIMATIC BOX PC 840. 




The new PC option considerably improves the functionality of the SIMATIC BOX PC 840.
The new drive permits:

  • reading of CD ROMs
  • reading and writing of CD R/RW
  • reading of DVD media.

Reading of DVD media enables even better linking of the Box PC to multi-media applications. The CD write function permits a convenient data transfer to cartridge media, which is often required  for data saving. The new drive is a Slimline-Combo drive as used in notebook computers, to ensure maximum robustness for this kind of product.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.