×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 12276904, Entry date: 06/10/2003
(0)
Rate

Transferring an NC block (traversing program) by user program to an FM353 / FM354

  • Entry
  • Associated product(s)

QUESTION:
How can I transfer an NC block (traversing program) by user program to an FM353 / FM354?

ANSWER:
In order to transfer a new or modified NC block to an FM 353 / FM 354 you program the Write job "Change parameters/data" in your user program.
Below is an example of how to assign the data record for transferring new NC blocks.

Assigning the user data block for transferring NC blocks:

The structure of the data record for the Write job "Change parameters/data" consists of

  • A data record header (in the manual: system data "Change parameters/data") and
  • The NC block (in the manual: system data "Active NC block").

For transferring the NC block

  • N20 G90 X400.000 [mm] F5000.000 [mm/min] M20

to traversing program no. 2 you have the following assignment in the user data block:

Address in the user DB

Name

Type

Value

Comment

Data record header

DBB 196

PAR_CHAN.TYP

BYTE

B#16#04

DB type: 4, traversing program

DBB 197

PAR_CHAN.NUMB

BYTE

B#16#02

Program no. 2

DBB 198

PAR_CHAN.COUN

BYTE

B#16#14

NC record no.: 20

DBB 199

PAR_CHAN.JOB

BYTE

B#16#02

Job type: 2, write parameters

NC block

DBB 200

PAR_CHAN.DATA[200]

BYTE

B#16#02

Program no. 2

DBB 201

PAR_CHAN.DATA[201]

BYTE

B#16#14

NC block no.: 20

DBX 202.0

BOOL

TRUE

Enable bit for G function group 1

DBX 202.1

BOOL

FALSE

Enable bit for G function group 2

DBX 202.2

BOOL

FALSE

Enable bit for G function group 3

DBX 202.3

BOOL

FALSE

DBX 202.4

BOOL

TRUE

Enable bit for Position / Dwell time

DBX 202.5

BOOL

FALSE

Enable bit for subprogram no.

DBX 202.6

BOOL

FALSE

Enable bit for number of subprogram calls

DBX 202.7

BOOL

FALSE

Enable bit for skippable block

DBX 203.0

BOOL

TRUE

Enable bit for speed

DBX 203.1

BOOL

TRUE

Enable bit for M function group 1

DBX 203.2

BOOL

FALSE

Enable bit for M function group 2

DBX 203.3

BOOL

FALSE

Enable bit for M function group 3

DBX 203.4

BOOL

FALSE

Enable bit for tool offset no.

DBX 203.5

BOOL

FALSE

DBX 203.6

BOOL

FALSE

DBX 203.7

BOOL

FALSE

DBB 204

PAR_CHAN.DATA[204]

BYTE

B#16#5A

G function 1: 90

DBB 205

PAR_CHAN.DATA[205]

BYTE

B#16#00

G function 2:

DBB 206

PAR_CHAN.DATA[206]

BYTE

B#16#00

G function 3:

DBB 207

PAR_CHAN.DATA[207]

BYTE

B#16#00

DBD 208

DINT

L#400000

Position in the MSR unit [µm]

DBD 212

DINT

L#5000000

Speed in the MSR unit / min

DBB 216

PAR_CHAN.DATA[216]

BYTE

B#16#14

M function 1: 20

DBB 217

PAR_CHAN.DATA[217]

BYTE

B#16#00

M function 2:

DBB 218

PAR_CHAN.DATA[218]

BYTE

B#16#00

M function 3:

DBB 219

PAR_CHAN.DATA[219]

BYTE

B#16#00

Tool offset no.

Table 1: Assignment of the data record structure for transferring an NC block

Notes on the user block:

  • Program no. and record no. are to be entered in the data record header and in the NC block.
  • An NC block must always be completely specified.
  • There is an enable bit and an input field for each block element of an NC record. For unused block elements you must set the enable bit and input field to "0" (see "Block structure" traversing blocks for a description of the block elements).
  • The position and speeds are to be specified in the unit of the measuring system. The following holds for the NC block above:
    input via traversing program editor:
    N20 G90 X400.000 [mm] F5000.000 [mm/min] M20
    input via user DB:
    N20 G90 X400000 [µm] F5000000 [µm/min] M20

Procedure for transferring an NC block from the user program to an FM 353/354:

  1. Transferring the new data into the data record DBB 196 ... DBB 219.
  2. Executing the Write job by setting the trigger bit DBX39.3.

Error evaluation:

If the module detects a data error, this is reported via the bit DBX 22.4 (data error). The cause of the error is entered in bytes DBB 94 (error class) and DBB 95 (error number).

Note:
The description applies for the standard blocks of the configuration package for FM 353 / FM 354, from version V3.1.

More information on the user data block and traversing blocks is available in the manual FM 353 - Entry ID 2106357 and FM 354 - Entry ID 2110628:

- Structure of the user data block

section 6.5

- System data "Change parameters/data"

section 9.3.1

- System data "Active NC block"

section 9.3.12

- Traversing blocks "Block structure"

section 10.1



Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.