×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 12378422, Entry date: 08/31/2005
(0)
Rate

Why can't you communicate with SCADA software (WinCC) using SIMATIC MicroComputing V1.0 and the EM241 modem module?

  • Entry
  • Associated product(s)

Description:
MicroComputing V1.0 does not support modem communication. However, S7-200 and WinCC do support the MODBUS protocol.

SIMATIC MicroComputing offers access to the process data in the S7-200 CPU and establishes the connection via ActiveX controls.

The EM241 modem module offers the "Remote communication" function for the S7-200 micro PLC and supports the following four operating mode:

  • Micro/Win connection for remote programming and trouble-shooting,
  • MODBUS master/slave communication,
  • alphanumerical messages and number call service,
  • as well as CPU-CPU communication between S7-200 micro-controllers.

For further information, please refer to the FAQs on "Possible ways of communicating with an S7-200 from WinCC V5.1", which you can find on the Internet under Entry ID: 21382197.

Remedy:
The HMI ‘WinCC’ software can be used as a MODBUS master and the EM241 modem module can be used as a MODBUS slave. Communication can be established this way between WinCC and the S7-22x CPU module via a telephone line.

Keywords:
Data transfer, Microcomputing, WinCC, Modem, S7-200


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.