×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 12642848, Entry date: 10/09/2002
(2)
Rate

Service Pack 6 for STEP 7 V5.1, STEP 7 Professional Edition 08/2000 and Edition 08/2001

  • Entry
  • Associated product(s)
Service Pack 6 for STEP 7 V5.1, STEP 7 Professional Edition 08/2000 and Edition 08/2001

DESCRIPTION:
Service Pack 6 for STEP 7 V5.1 is now available. 

Preconditon for the installation:

  • STEP 7 V5.1
  • STEP 7 Professional Edition 08/2000 
  • STEP 7 Professional Edition 08/2001

Please also note the information we have compiled for you in entry ID 12643072

Clients with a valid Software Update Service agreement ( SUS ) for STEP 7 will automatically receive a CD ROM with STEP 7 V5.1 incl. SP6.

Clients with a valid Software Update Service agreement ( SUS ) for STEP 7 Professional will automatically receive a CD ROM with the STEP 7 Professional Edition 08/2001 Release 10/2002. The SP6 for STEP 7 V5.1 is part of this Professional CD ROM ( see entry ID 12644828 ).

Clients without a valid Software Update Service agreement can obtain the CD ROM as follows:

  1. Place an order with your partner at Siemens:
    You can order the CD ROM with STEP 7 V5.1 incl. SP6 from your SIMATIC contact at your local Siemens office at a nominal charge. The order no. is: S79220-A6320-F

    A separate CD ROM is available for the new STEP 7 Professional Edition 08/2001. This CD ROM with the STEP 7 Professional Edition 08/2001 Release 10/2002 includes the SP6 for STEP 7 V5.1 and is available at a nominal charge only from your SIMATIC contact at your local Siemens office. The order no. is: S79220-A6325-F.
  2. Free Download
    As usual, we are also offering you  a free download. However, please not the size of the files.

     STEP7_V5_1_SP6.zip ( 120881 KB )

    This free download includes only the SP6 for STEP 7 V5.1. It does not contain STEP 7 V5.1 and also not NCM. There have not been any changes concerning NCM. If you have installed STEP 7 V5.1 incl. SP4 already, you do not require an update for NCM. 

    If you have installed STEP 7 V5.1 incl. SP3, please note the information about Hotfix 1 of NCM S7 for PROFIBUS and Industrial Ethernet V5.1 SP3 in the publication with entry ID: 11598916.

 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.