×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 13063839, Entry date: 02/15/2008
(3)
Rate

Why does the online mode not work with the S5-PC converter TTY - RS 232?

  • Entry
  • Associated product(s)

Description:
The converter requires a power supply of +5 V on PIN 14, which is supplied by the controller interface.
This power supply is ensured with the following devices: 

  • AG90U/95U/100U/101U/115U/115H/
  • AG135U/155U  (CPU921, 920, 922, 928A, 928B, 923, 947, 947R, 948)
  • CP530
  • IP252 (only AG115)
  • IP262

The pin assignment for the PC converter (MLFB 6ES5 734-1BD20) is displayed in the following figure:

Fig. 1: interface assignment of the PC converter ( 6 KB )  

Note:
Another cause might be that the device is equipped with a low-power interface. These interfaces provide much smaller voltages and currents on the send lines than normal RS232 interfaces. These interfaces are used on the RS232 side in many laptops/desktops and also in some USB adapters. For more information please refer to the manufacturer concerned.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.