×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 13336639, Entry date: 01/14/2019
(15)
Rate

How do you incorporate an operator panel created with WinCC flexible 2008 into a local network in order to save archive data on the PC?

  • Entry
  • Associated product(s)
An example to explain how to integrate an operator panel into a network. Other network constellations are possible, but these generally require further knowledge of networks.

Via Entry ID:92346478 you find a detailed application example for the WinCC (TIA Portal) entitled "Integrating HMI Operator Panels in TCP/IP Networks and access to a NAS or to a shared Windows folder".  

The enclosed documentation covers the following points.

Contents
1     Setting Up a Network Connection 
1.1  Assigning a Fixed IP Address 
1.2  Network Configuration on the Operator Panel
1.3  Additional Settings on the PC (Optional)
2     Enabling PC Network Sharing 
2.1  Archiving Path 
2.2  Share a File Folder or a Drive on a PC
2.3  Note on Windows 10

Documentation
  Documentation (1,1 MB)

Note
See the following entry for how to control a printer via the network: 18720136.

Additional Keywords
GMP, Pharma, Life Science, Validation, FDA 21 CFR Part 11

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.