×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 13336639, Entry date: 08/23/2016
(13)
Rate

How do you integrate an HMI operator panel into a local network?

  • Entry
  • Associated product(s)
This entry uses a simple example to explain how to integrate an operator panel into a network. Other network constellations are also possible, but these generally require further knowledge of networks.

Instructions
The example below explains how to

  1. Incorporate an operator panel into a local network in order to back up a tag archive to a PC via the local network.
  2. Share a folder or a drive on a PC.
  3. Save a tag archive to a PC via a local network.
  4. Access the files of the Comfort Panel from the PC.

 Procedure for WinCC (TIA Portal) and Windows 7 (651,7 KB) 

Contents
1. Overview
2. Setting Up a Network Connection
    2.1 Assigning a Static IP Address in Microsoft Windows 7
    2.2 Network Configuration on the Operator Panel
    2.3 Additional Settings on the PC
    2.4 Testing the Network Connections
3. Enabling Sharing
4. Saving the Tag Archive
5. Accessing the Files of the Comfort Panel

 Procedure for WinCC flexible and Windows XP (1,1 MB) 

Contents
1. Setting Up a Network Connection
    1.1 Assigning a Fixed IP Address in Microsoft Windows XP
    1.2 Network Configuration on the Operator Panel
    1.3 Additional Settings on the PC
    1.4 Testing the Network Connection
2. Enabling Sharing
3. Saving the Tag Archive

Note
For activating a printer over the network, for example, (see Entry ID: 18720136) addressing must also take place through a "name resolution".

Additional Keywords
GMP, Pharma, Life Science, Validation, FDA 21 CFR Part 11

 

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.
ProductSupport.EntityResultListTitle
ProductSupport.EntityResultListDescription

ProductSupport.EntityResultListButtonText
Copy URL
mySupport Cockpit
Related links