×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 14188898, Entry date: 02/25/2013
(6)
Rate

Which HMI components can you connect with S7-200 CPU and what should you watch out for when doing so?

  • Entry
  • Associated product(s)

Configuration Notes:  
You can connect a SIMATIC S7-200 CPU with different types of HMI devices. Here you must take into account differences in communications protocols, baud rates and the number of connections possible. The HMI device always plays the active part in the communication. This entry covers the following two aspects:

One HMI component with multiple SIMATIC S7-200 CPUs
Below is an overview of HMI components that can be connected with the SIMATIC S7-200. In the following table "Number of S7-200s" stands for the maximum number of S7-200 controllers that can be parameterized with the configuration tool. Unless otherwise marked in the table the maximum baud rate is

  • 187.5 Kbit/s with PPI protocol
  • 12.0 Mbit/s with MPI protocol
HMI components Configuration tool1) Number of S7-200s with
PPI protocol
Number of S7-200s with
MPI protocol
 S7-200 via CP243-1
Ethernet
PP 7 Configuration tool not required - 1 (max. 1.5 Mbit/s)  -
PP 17-I Configuration tool not required - 1 (max. 1.5 Mbit/s)  -
PP 17-II Configuration tool not required - 1 (max. 1.5 Mbit/s)  -
TD 17 As from ProTool / Lite V2.51 4 4 -
OP 3 As from ProTool / Lite V2.51 2 2 5) -
OP 5 As from ProTool / Lite V1.01 4 2 5) -
OP 7 As from ProTool / Lite V2.5 4 4 -
OP 15 As from ProTool / Lite V1.01 4 4 5) -
OP 17 As from ProTool / Lite V2.5 4 4 -
OP 25 As from ProTool V1.31 4 4 (max. 1.5 Mbit/s)  -
OP 27 As from ProTool V3.1 4 4 -
OP 35 As from ProTool V1.31 6 6 (max. 1.5 Mbit/s)  -
OP 37 As from ProTool / Lite V2.5 8 8 -
TP 27  As from ProTool V3.1 4 4 -
TP 37  As from ProTool V3.1 8 8 -
TP 070 As from TP Designer version V1 - 1 (max. 19.2 Kbit/s)  -
OP 73 Micro As from WinCC flexible 2004 Micro SP1+HSP1.1 1 1 (max. 187.5 Kbit/s) 2) -
TP 170micro As from WinCC flexible 2004 Micro 1 1 (max.187.5 Kbit/s) -
TP 177micro As from WinCC flexible 2004 Micro SP1+HSP1.1 1 1 (max. 187.5 Kbit/s) 2) -
Mobile Panel 170 As from ProTool / Lite V6.0 SP 2, WinCC flexible 2004 Compact 1 4 -
Mobile Panel 177 DP As from WinCC flexible 2005 Compact 1 4 -
Mobile Panel 177 PN As from WinCC flexible 2005 Compact - - 4 4)
Mobile Panel 277 As from WinCC flexible 2005 SP1 Standard 1 8 8 4)
OP 73 As from WinCC flexible 2004 Compact SP1+HSP1.1 1 2 (max. 1.5 Mbit/s) 2) -
OP 77A As from WinCC flexible 2004 Compact SP1+HSP1.1 1 4 (max. 1.5 Mbit/s) 2) -
OP 77B As from WinCC flexible 2004 Compact 1 4 -
TP 170A As from ProTool V6.0 1 1 (max. 1.5 Mbit/s)  -
TP 170A As from WinCC flexible 2004 Compact 1 4 (max. 1.5 Mbit/s)  -
TP 177A As from WinCC flexible 2004 Compact SP1+HSP1.1 1 4 (max. 1.5 Mbit/s) 2) -
TP 170B As from ProTool V6.0, WinCC flexible 2004 Compact 1 4 -
TP 177B 4" PN/DP COLOR As from WinCC flexible 2008 Compact 1 4 4 4)
TP 177B DP As from WinCC flexible 2005 Compact 1 4 -
TP 177B PN/DP As from WinCC flexible 2005 Compact 1 4 4 4)
OP 170B As from ProTool / Lite V5.2 SP 2, WinCC flexible 2004 Compact 1 4 -
OP 177B DP As from WinCC flexible 2005 Compact 1 4 -
OP 177B PN/DP As from WinCC flexible 2005 Compact 1 4 4 4)
TP 270, OP 270 As from ProTool V6.0 SP 3, WinCC flexible 2004 Standard 1 8 8 4)
TP 277, OP 277 As from WinCC flexible 2005 Standard SP1 1 8 8 4)
MP 177 As from WinCC flexible 2008 Standard 1 8 8 4)
MP 270 As from ProTool V6.0 1 8 8 4)
MP 270B As from ProTool V6.0 SP 3, WinCC flexible 2004 Standard 1 8 8 4)
MP 277 As from WinCC flexible 2005 Standard SP1 1 8 8 4)
MP 370 Key As from ProTool V6.0 SP 3, WinCC flexible 2004 Standard 1 8 8 4)
MP 370 Touch As from ProTool V6.0 SP 2, WinCC flexible 2004 Standard 1 8 8 4)
MP 377 As WinCC flexible 2005 Standard SP1 1 8 8 4)
PC IL 70 ProTool/Pro CS, WinCC flexible Advanced 1 8 (max. 187.5 Kbit/s)  8 4)
PC IL 77, PC 477,
PC 577, PC 670,
PC 677, PC 870,

PC 877
ProTool/Pro CS, WinCC flexible Advanced 1 8 8 4)
PCs ProTool/Pro CS, WinCC flexible Advanced 1 8 8 4)
FI 25 ProTool/Pro CS 1 8 (max. 1.5 Mbit/s)  -
FI 45 ProTool/Pro CS 1 8 -
OP 37 Pro Configuration set 1 8 -
TD 100C, TD200, TD200C, TD400C 3) Text display wizard of STEP 7 Micro/WIN 1 1 (max. 187.5 Kbit/s)  -
KTP400 Basic Mono PN,
KTP600 Basic Mono PN,
KTP600 Basic Color PN,
As from WinCC flexible 2008 Compact SP1 - - 4 4)
KTP600 Basic Color DP As from WinCC flexible 2008 Compact SP1 1 1 -
KTP1000 Basic Color DP As from WinCC flexible 2008 Compact 1 4 -
KTP1000 Basic Color PN,
KTP1500 Basic Color PN
As from WinCC flexible 2008 Compact - - 4 4)
1)

The required tool specified, if specified separately, is the minimum requirement with regard to release, version, service pack or HSP on the one hand and the tool version "Lite", "Compact", "Standard", etc. on the other hand.

2)

The HMI device can also communicate with an PPI master in the same network, if only S7-200 connections are configured in the project for it. This is the exception. An MPI master cannot usually access a PPI master in the same network.

3) TD 200: the text display sets itself automatically to the protocol concerned.
4) Only one HMI component can communicate with the S7-200 at any one time (on account of the connection management via TSAP).
5) As from ProTool/Lite 3.0 and ProTool 3.0 you can also select the MPI and PROFIBUS protocol for OP3, OP5, OP15A and OP15C.

Note:  
An MPI master cannot usually access a PPI master in the same network.

One SIMATIC S7-200 CPU with multiple HMI components
Communication can be via the MPI or PPI protocol.

  • In the case of the MPI protocol the CPU communicates with each HMI device via a separate connection. This effectively avoids communication problems. However, the number of HMI devices that you can connect to an S7-200 CPU is greatly limited and depends on the type of CPU. The following table gives an overview.
     
    MPI (DP/T) Number of HMI comp.
    CPU Port 0
    Max. baud rate

    CPU Port 0

    Number of HMI comp.
    CPU Port 1
    Max. baud rate

    CPU Port 1

    Number of HMI comp.
    EM 277 Port
    CPU 212
    (as from firmware 1.1)
    3 19.2 kbit/s - - -
    CPU 214
    (as from firmware 1.1)
    3 19.2 kbit/s - - -
    CPU 215 3 19.2 kbit/s 5 12 Mbit/s  -
    CPU 216 3 19.2 kbit/s 3 19.2 kbit/s -
    CPU 221 3 187.5 kbit/s - - -
    CPU 222 3 187.5 kbit/s - - -
    CPU 224 3 187.5 kbit/s - - -
    CPU 224XP 3 187.5 kbit/s 3 187.5 kbit/s  
    CPU 226 3 187.5 kbit/s 3 187.5 kbit/s -
    EM 277 - - - - 5 / 
    max.12 Mbit/s 

Special case:
You can connect up to 3 pushbutton panels of the same type (PP7, PP 17-I or PP 17-II); these then all have the same functionality. You assign parameters to the pushbutton panels via the data block of the controller. S7-200 has only one data block and therefore multiple functions cannot be provided for the panels (Entry ID: 691006).

Note: 
Only one TP 070 without any other nodes may be connected to each CPU interface.

  • In the case of the PPI protocol, you can theoretically connect 32 nodes, that is a maximum of 32 HMI devices. However, with PPI in one time interval there is only ever one logical connection between the nodes (time multiplex), which is established and disconnected for each communication. The baud rate is max. 187 kbit/s. This practically reduces the number of HMI devices to three per interface.
    Now, in PPI mode, if several HMI devices (PPI masters) access the CPU (PPI slave), it might happen that an HMI device constantly arrives at the CPU that is occupied by another HMI device (or by another PPI master) and is no longer updated. In this case, you should increase the update cycles of the HMI devices. You do this in the relevant configuration tools of the HMI devices or with the text displays TD 100/200(C) in the Micro/WIN text display wizard.
    Use Advanced PPI if the master concerned supports it. This type of protocol uses a separate connection like MPI. For example, when setting the PG/PC interface in Micro/WIN, you can select Advanced PPI when choosing a PPI connection.

More information on communication protocols of the S7-200 is available in the "S7-200 System Manual", chapter 7 - Communicating over a Network, in Entry ID: 1109582 .

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.