×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 142591, Entry date: 08/29/2003
(0)
Rate

Memory concept of the AG 95

  • Entry
  • Associated product(s)

QUESTION:
How large is the memory of the AG 95 and how can I use it?

ANSWER:
The following versions of the S5-95 U with a second interface have memories of 20 KB:

S5-95U with SINEC L2 interface 6ES5 095-8MB02 as of Version A02
S5-95U with second serial interface 6ES5 095-8MC01 as of Version A04
S5-95U with SINEC L2 DP slave interface 6ES5 095-8MD01 as of Version A02
S5-95U with SINEC L2 DP master interface 6ES5 095-8ME01 as of Version A01

Of the 20 KB user memory of the AG 95 you can use up to 16 KB for your user program.
At least 4 KB must be reserved for data blocks.
The blocks can be transferred to the PLC in random order.
The versions with just one interface (PG interface) have a memory of 16 KB:

S5-95U Basic Unit 6ES5 095-8MA03 as of Version A01

You can use the 16 KB of user memory as you wish for program and data blocks.

Note:
The AG 95F owns a user memory of 16KB, from which 8 KB are reserved for the data and 8 KB are reserved for the application. This applies for every AG 95F!


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.