Entry type: FAQ, Entry ID: 14328197, Entry date: 02/05/2003
(0)
Rate

Why can no OS be inserted in the SIMATIC Manager when using STEP 7 V5.2 and WinCC V5.1?

  • Entry
  • Associated product(s)

Description:  
When you want to operate WinCC V5.1 and STEP 7 V5.2 together on an PG/PC, the HF 0 to WinCC V5.1 is obligatory. It is - independent of perhaps already installed hotfixes for WinCC V5.1 - installable via Setup.
You can find the hotfix setup in the folder "WinCC-Hotfix"; in the STEP 7 V5.2 CD.

Two orders of installation are possible:

1. WinCC V5.1 -> STEP 7 V5.2 -> Hotfix 0 for WinCC V5.1

or

2. STEP 7 V5.2 -> WinCC V5.1-> Hotfix 0 for WinCC V5.1 

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster