×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 14340592, Entry date: 06/22/2010
(1)
Rate

Why is the voltage output of the S7-300 and S7-400 analog output group outside of the tolerance? What are the terminals S+ and S- used for?

  • Entry
  • Associated product(s)

Description
The following description applies to all SM 332 and SM 432 analog output modules.

The allocation for return inputs S+ and S- needs to be observed when using the SM 332 and SM 432 analog output modules. They serve the purpose of compensating the line resistance. When you connect the two contacts of the actuator with separate wires with the S+ and S-, the analog output adjusts the output voltage, so that the desired output voltage actually exists on the actuator. 

If the compensation is desired, the actuator must be connected with four wires. For example, for the analog output module 6ES7332-7ND02-0AB0 and for the first channel this means: 

  • You must conduct the output voltage from Pin 3 and Pin 6 to the actuator.

  • Sensor leads SO- and SO+ must be conducted directly from the actuator to Pin 4 and Pin 5. 


Fig. 01

If compensation is not desired, simply bridge the Pins 3-4 and 5-6 on the front connector.

Note
In the case of open sensor leads (S+ and S-), the output voltage is readjusted by a maximum of 140 mV (for 10V).
For this connection configuration, the operational limit of ± 0.5 % for the voltage output cannot be kept.

Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.