Entry type: FAQ, Entry ID: 14668901, Entry date: 06/10/2010
(0)
Rate

What settings are to be made when connecting a printer to a Windows-based panel?

  • Entry
  • Associated product(s)

Configuration:
Except in the case of an Ethernet connection, the printer is configured entirely in the Control Panel of the SIMATIC HMI operator panel.

  • Double-click on the "Printer" icon and the printer configuration dialog opens.


Fig. 01
 

Printer Language Choice of printer
Port Interface
Network Network address of the printer
Paper Size Paper format
Orientation Alignment of the printout
Draft Mode / Color / CMY Print quality
Table 01: Explanation

Serial port RS232

  • You must set the printer language, printer port, paper size, orientation (portrait or landscape), color or black-and-white print and the quality of the printout.
  • Use the IF2 or IF1A port for connecting the printer via the serial interface. The pin assignments are also in the Printer list.


Fig. 02

Notes:
In order to be able to use the serial interface on the operator panel (IF 2) for communication with the printer, you must clear the check mark for "Remote Control" under "Serial" in the "Transfer Settings" dialog.

Please refer to the Printer list at the end of this entry for the printer settings of the printers released.

USB interface

  • You must set the printer language, printer port, paper size, orientation (portrait or landscape), color or black-and-white print and the quality of the printout.
  • Use the USB1 port for connecting the printer via the USB interface.


Fig. 03

Note:
Please refer to the Printer list at the end of this entry for the printer settings of the printers released.

Ethernet interface - Network printer

  • The settings required to print with a SIMATIC HMI operator panel on a network printer are given in Entry ID: 18720136.

 
Fig. 04

Ethernet interface - Print server (as from WinCC Flexible 2008 SP1)

  • You must set the printer language, printer port, paper size, orientation (portrait or landscape), color or black-and-white print and the quality of the printout.
  • You must select the "PrintSever" port for printing on a print server via Ethernet.
  • In the "IP:Port:" input field you enter the IP address and the port for communication with the print server.
    Use ":"as separator character between IP address and port; for example: "192.168.56.23:9100"
  • The print server uses the "RAW" mode.


Fig. 05

Note:
Please refer to the Printer list at the end of this entry for the printer settings of the printers released.

  • In this case, the operator panel must be configured for network operation. The necessary settings are in the device manual concerned in each case.
    Entry ID: 13336639 also includes instructions for how to integrate an operator panel in a network.
The following SIMATIC HMI operator panels support printing via a print server:
  • xP 177, Mobile Panel 177
  • xP 277, Mobile Panel 277, Mobile Panel 277 IWLAN, Mobile Panel 277F IWLAN
  • Mobile Panel 277 IWLAN V2, Mobile Panel 277F IWLAN V2, Mobile Panel 277F IWLAN (RFID Tag)
  • MP377

Printer list:
The following entry includes the official printer list of all the printers that are released for use with SIMATIC operator panels. Also included are all the cables that can be used plus their pin assignments.
"Released Printers for SIMATIC Panels and Multi Panels", Entry ID 11376409.

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster