×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 14747677, Entry date: 04/27/2015
(0)
Rate

Which modules support clock-synchronized operation on the PROFIBUS-DP?

  • Entry
  • Associated product(s)
Clock synchronicity with PROFIBUS DP is used to establish a direct connection between the equidistant DP cycle, the IO modules and the user program.

Description
The list below shows which modules support clock-synchronized operation as PROFIBUS DP master.
 
 14747677_PROFIBUS_DP_Taktsynchronität_en.pdf (69,8 KB) 

You can only use the internal DP interfaces of the CPUs for clock-synchronized communication with PROFIBUS DP.
You can use STEP 7 V5.2 and higher or TIA Portal for configuring.

The clock synchronicity is also supported by the complete product group "SIMODRIVE 611U", "SINAMICS" and "MASTERDRIVE MC". The following are required in order to configure the drives: Drive ES Basic V5.2 or higher, STEP 7 V5.2 or higher and one of the CPUs mentioned above.

Additional Information

  • More information about clock synchronicity is available in the manual entitled "SIMATIC PROFINET System Description" in Entry ID 19292127

Additional Keywords
Constant bus cycle time, Compatibility list

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.