×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 15206303, Entry date: 05/05/2003
(0)
Rate

Microsoft Windows language versions released for SIMATIC WinCC V5.1

  • Entry
  • Associated product(s)

QUESTION:
Which Microsoft Windows language versions are released for SIMATIC WinCC V5.1?

ANSWER:  
WinCC V5.1 supports German, English, French, Italian and Spanish.
Microsoft Windows NT 4.0 and Windows 2000 are the operating systems released in the following languages:

  • German
  • English
  • French
  • Italian
  • Spanish

It is also possible to use Windows 2000 MUI for the languages listed above with the appropriate LanguagePack.

The Windows Service Packs released for WinCC V5.1 are listed in Entry ID: 1139080.

Note:
For WinCC V5.1 ASIA please refer to the information given in Entry ID: 15093581.

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.