×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 15284538, Entry date: 05/18/2009
(0)
Rate

How can you install WinCC while the computer is logged on to a domain?

  • Entry
  • Associated product(s)

Description:
In SIMATIC WinCC, it is not possible to do an installation of WinCC while the computer is logged on to a domain.

Instructions:

  • Log on locally with administrator rights to the computer in question. An installation under the Microsoft Windows operating system requires administrator rights.
  • Refer to the requirements for installation in the SIMATIC WinCC Installation Notes or in the relevant section of the WinCC Information System. 
  • Once the installation is finished, you can log on to the domain again as usual.

Note:
More information regarding the use of WinCC systems on a domain is available in the WinCC Information System under the keyword "Domain".
Information on the installation of WinCC can be found in the WinCC Information System under "Installation Notes > Requirements for Installation".

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.