×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 15364845, Entry date: 06/10/2003
(0)
Rate

Connecting a ProTool Runtime Panel / PC to an S7 200 via PROFIBUS DP

  • Entry
  • Associated product(s)

QUESTION:
Which settings have to be made for a PROFIBUS DP link between a Panel or PC with the ProTool/Pro-Runtime and the S7-200?

ANSWER:  
If you want to connect a ProTool Runtime device to an S7-200, please make sure that the S7-200 can be operated only as a DP slave. The Panel or PC has to be implemented as DP master on the PROFIBUS DP network and the S7-200 as DP slave.

The following settings have to be made:

ProTool

  • In ProTool you configure a PLC connection to the S7-200.
  • Use "SIMATIC S7-200" as the protocol and open the "Parameters…".

Fig. 1: Select PLC protocol

  • To be able to set up a communication between the S7-200 as DP slave and the PC as DP master, you must check the option "Only Master on the Bus". 

Example: 
Five PCs are communicating via ProTool/Pro Runtime  and PROFIBUS DP with an S7-200. One PC is the DP master, i.e. the option "Only Master on the Bus" is checked only for this PC. The other PCs do not have a check mark set for the option "Only Master on the Bus". 

Now, if the master PC fails, communications on the PROFIBUS DP network break down completely, because there is no master on the bus. As soon as the master PC goes back online (ProTool/Pro Runtime is started and the PLC connection is active), then the other PC stations can again set up a connection to the S7-200. 

It is thus recommended to declare all PCs to be master by checking the option "Only Master on the Bus" for all the PCs, then communications are not dependent on one single PC. 

Fig. 2: Communications settings

In addition, you have to enter all the other settings for the PROFIBUS DP connection. By pressing the "More…" button you can specify the number of masters on the PROFIBUS DP. 

Fig. 3: Number of masters

Note: 
With a PC, the PG/PC interface has to be configured to "S7ONLINE --> PROFIBUS".

Fig. 4: PG/PC interface

STEP 7 - Micro/WIN

With STEP 7-Micro/WIN, the interface of the S7-200 has to be configured according to the parameters used in ProTool.

Notes:

  • For a PROFIBUS DP communication with a baud rate > 187.5 Kbaud you need a DP interface on the S7-200.
  • For the S7-22x without integrated DP interface you need an EM277 module for the PROFIBUS DP communication (Baud rate > 187.5 Kbaud).
  • More information on OP communications with S7-200 is available in Entry ID: 14188898 "S7-200 and HMI components".



Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.