Entry type: FAQ, Entry ID: 15386411, Entry date: 11/12/2013
(0)
Rate

How can you back up the data of the Windows event viewer?

  • Entry
  • Associated product(s)

Instructions:
Information, warnings and errors relating to hardware or the operating system are stored in the Microsoft Windows event viewer. For diagnosing it might be necessary to make the data of the event viewer available for the Siemens Technical Support.

Procedure in Windows NT 4.0
 

No. Procedure
1 Call the event viewer with "Start > Programs > Administration (General) > Event Viewer".
2 Using the menu item "Protocol > System" or "Protocol > Application" you can switch to the protocol concerned.
3 Save the data from both protocols in each case with "Protocol > Save as..." and select the file type *.EVT.
4 If possible, archive the stored protocols before sending them to Technical Support, for example in a .zip archive. This greatly reduces the volume of data to be transferred.
Table 01

Procedure in Windows 2000/2003 Server/XP
 

No. Procedure
1 Call the event viewer from the Control Panel with "Administrative Tools > Event viewer".
2 You can switch between log files for System and Applications in the tree structure in the window on the left.
3 Save the application log file and the system log file selecting *.EVT as file type.
4 If possible, archive the stored log files before sending them to Technical Support, for example in a .zip archive. This greatly reduces the volume of data to be transferred.
Table 02

Procedure in Windows Vista/Windows 7/2008 Server
 

No. Procedure
1 Call the event viewer.
Start > Control Panel > System and Security > Administrative Tools> Event Viewer    VIEW: Category or
Start > Control Panel > All System Control Elements > Administrative Tools> Event Viewer    VIEW: Large/small symbols
2 In the tree structure you switch to "Windows Logs" in the window pane on the left. Double-click to open this.
3 Select the subitem "Application" in the window pane on the left. Right-click to open the pop-up menu and select the "Save all events as..." function. Save the complete application protocol as an *.EVTX file.
Select the subitem "System" in the window pane on the left. Right-click to open the pop-up menu and select the "Save all events as..." function. Save the complete system protocol as an *.EVTX file.
4 If possible, archive the stored log files before sending them to Technical Support, for example in a .zip archive. This greatly reduces the volume of data to be transferred.
Table 03

Collecting diagnostics files centrally
How to gather together the diagnostics and system information of your computers on one central computer is described in Entry ID 65976201.