Entry type: FAQ, Entry ID: 1548652, Entry date: 11/26/1999
(0)
Rate

EasyLanguage adds a 'T' to empty ToolTips upon export

  • Entry
  • Associated product(s)

QUESTION:
Why, after importing the updated csv file with EasyLanguage, do all the previously empty ToolTips have a 'T'?

ANSWER:
This behavior occurs in versions of EasyLanguage < V5.0. When the image texts are exported into a csv-file with the EasyLanguage versions concerned, then a 'T' is added to all empty ToolTip fields. The current version V5.0 of EasyLanguage is on the WinCC V5 CD in the SmartTools -> CC_GraphicsTextImportExport path.

If you are using an older version of EasyLanguage and this case occurs, then there is a quick way of getting rid of the "T":

  1. After import, select all the operable objects.
  2. Then remove the ToolTip for all of them together.
Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster