×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 16540057, Entry date: 07/22/2003
(4)
Rate

Service Pack 1 for STEP 7 V5.2 and STEP 7 Professional Edition 12/2002

  • Entry
  • Associated product(s)
Service Pack 1 for STEP 7 V5.2 and STEP 7 Professional Edition 12/2002


DESCRIPTION:

Download of Service Pack 1 for STEP 7 V5.2

Preconditions for the installation:

  • STEP 7 V5.2
  • STEP 7 Professional Edition 12/2002

Please also read the information (What is New, special hints, etc.) we have compiled for you under entry ID 16540054 .

Clients with a valid Software Update Service agreement (SUS) for STEP 7, will receive the CD ROM with STEP 7 V5.2 incl. SP1 automatically.

Clients with a valid Software Update Service agreement (SUS) for STEP 7 Professional, will receive the CD ROM with the STEP 7 Professional Edition 012/2002, Release 07/2003 automatically.
The SP1 for STEP 7 V5.2 is also part of this Professional CD ROM (see entry ID 16535207 )

The following options are available to clients without a valid SUS agreement:

  1. Place an order with your local Siemens partner
    You can order the CD ROM with STEP 7 V5.2 incl. SP1 from your local Siemens partner at a nominal fee. The order no. is: S79220-A6575-F

    A separate CD ROM is available for the current STEP 7 Professional Edition 12/2002. This CD ROM with the STEP 7 Professional Edition 12/2002 Release 07/2003 also includes the SP1 for STEP 7 V5.2 and can also be ordered from your local Siemens partner at a nominal fee. The order no. is: S79220-A6656-F.
  2. Free download
    As usual, we are offering a free download. However, please note the file size.

    STEP7_V5.2_SP1.zip ( 102231 KB )

    This free download only contains the SP1 for STEP 7 V5.2, i.e. neither STEP 7 V5.2 nor NCM.

    The CD ROM for STEP 7 V5.2 incl. SP 1 also includes the Service Pack 1 for NCM S7 V5.2.



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.