×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 16697502, Entry date: 04/01/2008
(0)
Rate

How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?

  • Entry
  • Associated product(s)

Instructions:
In this example, a standard Ethernet network card is used for the S5-compatible communication with the S5 station using the FETCH and WRITE services via the OPC server.

Note:
The procedure described here also applies for communication processors CP1613, CP1512 and CP1612.

General Information:
You can choose between two different configuration tools:

  • NCM PC: 
    NCM PC is supplied with the SIMATIC NET CD and permits you to create PC projects and open STEP 7 projects. However, it is not possible to use this software to edit the S7 blocks in the STEP 7 project.
  • STEP 7:  
    STEP 7 is a separate software package and permits you to create S7-400, S7-300 and PC projects. It is possible to use this software to edit the S7 blocks.

Only one of these tools can be installed.

Please follow the instructions below for configuring the PC station.

Guideline_FW_S5_e.pdf ( 2024 KB )

Keywords:  
Fetch/Write connection, Configuration, Guideline, OPC Server, SOFTNET S7, SOFTNET S7 Lean, S7-1613

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.