×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 16800008, Entry date: 08/25/2003
(0)
Rate

Establishing an Ethernet connection for APT ONLINE functions with SIMATIC NET 11/2002 and CP1613

  • Entry
  • Associated product(s)

QUESTION:  
What has to be watched out if I want to use a SIMATIC NET CD 11/2002 and a CP1613 for APT ONLINE functions?

ANSWER:
Make sure that in the configuration console for the CP 1613 under the entry "General","PG-operation" is set under Mode of the module.

All further steps are identical to the configuration using the SIMATIC NET CD 05/2000. The realisation of this configuration is described under entry ID: 16801401. Some of the illustrations may slightly look different, (especially the settings in the tool "Set PG/PC-interface") between the different SIMATIC NET CD editions. However, number and contents of the configuration dialog boxes are identic.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.