×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 17090003, Entry date: 09/23/2003
(0)
Rate

PROFIBUS connection of the S5 100 U via CP541 is possible

  • Entry
  • Associated product(s)

QUESTION:
Is there a possibility of connecting the S5 100 U with the PROFIBUS?

ANSWER:
A connection can be established with the CPU 541 to the PROFIBUS. The CP541 is connected with the first interface to the SINEC-L1 interface of the S5 100 U and with the second interface to the PROFIBUS.

The CP541 supports the bus profiles FDL, DP and FMS.

Note:
Further information concerning this unit can be found in the manual "Communication processor CP 541" under entry-ID: 1456021


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.