×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 17233995, Entry date: 10/07/2003
(0)
Rate

Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)

  • Entry
  • Associated product(s)

QUESTION:
Why doesn't the ET 200S module DI 4xNAMUR work when I configure it with STEP 7 V5.2?

ANSWER:
Due to changes in function the ET 200S module DI 4xNAMUR (6ES7 131-4RD00-0AB0) can only be configured completely with STEP 7 V5.2 SP1.

All modules that have already been configured with STEP 7 V5.2 without Service Pack have to be deleted and reconfigured with STEP 7 V5.2 SP1 or higher.

Keywords:
System requirements, Hardware configuration, ET 200S DI