Entry type: FAQ, Entry ID: 17233995, Entry date: 10/07/2003
(0)
Rate

Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)

  • Entry
  • Associated product(s)

QUESTION:
Why doesn't the ET 200S module DI 4xNAMUR work when I configure it with STEP 7 V5.2?

ANSWER:
Due to changes in function the ET 200S module DI 4xNAMUR (6ES7 131-4RD00-0AB0) can only be configured completely with STEP 7 V5.2 SP1.

All modules that have already been configured with STEP 7 V5.2 without Service Pack have to be deleted and reconfigured with STEP 7 V5.2 SP1 or higher.

Keywords:
System requirements, Hardware configuration, ET 200S DI


Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster