×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 17294496, Entry date: 11/27/2017
(0)
Rate

How do you count the number of process objects (PO) for the PCS 7 licenses?

  • Entry
  • Associated product(s)
The number of process objects (PO) is counted on the Engineering Station (ES). How you can read out the current number of process objects from your project is described in the entries below.
PCS 7 Version - ManualEntry IDChapter
 PCS 7 V9.0 - Engineering System109746533  Counting and booking process object licenses 
PCS 7 V8.2 - Engineering System109485969Counting and Booking Process Object Licenses
PCS 7 V8.1/ V8.1 SP1 - Engineering System90663380Counting and Booking Process Object Licenses
PCS 7 V8.0 SP1 / V8.0 SP2 - EngineeringSystem68157345Counting and Booking Process Object Licenses
PCS 7 V8.0 - Engineering System57270203Counting and Booking Process Object Licenses
PCS 7 V8.0 - Engineering System109485969Counting and Booking Process Object Licenses



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.