×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 17532609, Entry date: 12/20/2007
(0)
Rate

How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?

  • Entry
  • Associated product(s)

Instructions:
In this example, a standard Ethernet network card is used for the S7 communication via a user application with an S7 controller on the Industrial Ethernet.

Note:
The procedure described here also applies for communication processors CP1613, CP1512 and CP1612.

General information:
The requirement is that one of the two following configuration tools is installed.

  • NCM PC: NCM PC is supplied with the SIMATIC NET CD and permits you to create PC projects and open STEP 7 projects. However, it is not possible to use this software to edit the S7 blocks in the STEP 7 project.
     
  • STEP 7: STEP 7 is a separate software package and permits you to create S7-400, S7-300 and PC projects. It is possible to use this software to edit the S7 blocks.

Only one of these tools can be installed.

Please follow the instructions below for configuring the PC station.

Guide_S7_IE_Appl_e.pdf ( 1637 KB )

Keywords: 
OPC server, S7 connection, Industrial Ethernet, Guideline, Instructions, SOFTNET S7 IE, SOFTNET S7 Lean, S7-1613, Network card, Set up connection, SIMATIC NET PC software

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.