×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 17545812, Entry date: 12/15/2003
(2)
Rate

Hotfix 3 for STEP 7 V5.2 SP1 and STEP 7 Professional Edition 12/2002 Release 07/2003

  • Entry
  • Associated product(s)

DESCRIPTION:

Preconditions for the installation of the Hotfix:

STEP 7 V5.2 SP1 or STEP 7 Professional Edition 12/2002 Release 07/2003 must be installed. The authorization for STEP 7 V5.2 or STEP 7 Professional Edition 12/2002 will remain valid with the Hotfix 3.

What is the purpose of the Hotfix?

The Hotfix is required to be able to read and write the following new SIMATIC Micro Memory Cards (MMC) with SIMATIC programming devices:

MMC

Order No.

MMC 64 Kbyte

6ES7 953-8LF11-0AA0

MMC 128 Kbyte

6ES7 953-8LG11-0AA0

MMC 512 Kbyte

6ES7 953-8LJ11-0AA0

MMC 2 Mbyte

6ES7 953-8LL11-0AA0

MMC 4 Mbyte

6ES7 953-8LM11-0AA0

MMC 8 Mbyte

6ES7 953-8LP11-0AA0

It is not necessary to install the Hotfix if none of the above new Micro Memory Cards are to be used with the programming device. In the near future, STEP 7 version 5.3 and STEP 7 Professional Edition 2004 will include the required function as a standard. The new version of STEP 7 / STEP 7 Professional will be delivered within the scope of the Software Update Service as from the 1st quarter 2004.

Important: STEP 7 version 5.3 and STEP 7 Professional Edition 2004 will only be released for Windows 2000 Professional and Windows XP Professional operating systems.

Hotfix 3 for STEP 7 V5.2 SP1 and STEP 7 Professional Edition 12/2002 Release 07/2003
STEP7_V52_SP1_HF3.zip ( 30345 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.