×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 17581786, Entry date: 06/28/2010
(0)
Rate

Why does the CH_AI driver report the slave still to be defective (QBAD=1) after failure and return of a PROFIBUS DP slave (e.g. ET 200M)?

  • Entry
  • Associated product(s)

Description
One possible cause is that the properties of the CPU were wrongly set. Therefore, you should check in the HW Config under "Properties of the CPU > Tab: Cycle/Clock Memory > parameter "OB85 call upon I/O access error", whether "Only for incoming and outgoing errors" is set and change the setting if necessary.
This is the only way to make sure that the I/O access error (output parameter QPERAF) is evaluated correctly. Furthermore, you save cycle time, because repeated calling of the OB 85 can increase the cycle time.

This setting is absolutely mandatory when using the SIMATIC PCS 7 driver concept! Please also refer to Entry ID: 10331925.

Remark
With SIMATIC PCS 7 version V6.0, this is a default setting in the HW Config for all PCS7 projects.