×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 17624774, Entry date: 11/25/2003
(0)
Rate

External programming devices with USB interface in order to program memory modules for SIMADYN D and SIMATIC TDC

  • Entry
  • Associated product(s)

QUESTION:
Which external programming device do I have to connect to the USB interface of a PC or PG's, in order to program memory modules for SIMADYN D, FM458 and SIMATIC TDC offline (the FM 458-1 is not affected by this)?

ANSWER:
The programming of the program memory modules MS5, MS51, MS52, MC500, MC510 and MC521 for D7-SYS can be executed at a PC or PG with a USB interface via the external "OmniDrive USB LF".

This device can be obtained from CSM.
Please pay attention to the addition "LF" at the order.

CSM GmbH
Raiffeisenstr. 34
D-70794 Filderstadt
Tel.: +49 (0) 711-77964 -20
Fax: +49 (0) 711-77964 -40
eMail: info@csm.de
http://www.csm-products.com


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.