×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 17822754, Entry date: 12/10/2003
(0)
Rate

SIMATIC PCS7 V6 block for SINAMICS G150

  • Entry
  • Associated product(s)

Integrating a SINAMICS G150 drive into the SIMATIC PCS7 V6.0 process control system using Drive ES PCS7 V6.0



Order No. [MLFB]: 6SW1700-6JD00-0AA0 or 6SW1700-6JD00-0AA4

The Drive Engineering System (Drive ES PCS7) is used to integrate drives into the SIMATIC PCS7 process control system. Up until now, Drive ES PCS7 did not support the new SINAMICS G150 drive series. Effective immediately, a control block with picture block is available to integrate a SINAMICS G150 drive into SIMATIC PCS7 V6.

This block supplements the DRVPCS7 library of the Drive ES PCS7 V6.0 product.

In order to acquire the block, you have to be in position of Drive ES PCS7 V6.0. Please have the license number of your product ready and contact SIEMENS Automation and Drive Technology Customer Support (ad.support@siemens.com ). You will then receive the password so that you can extract the zipped archive which contains the block. The archive "DRVPCS7_SINA_60.zip" is provided as download together with this info.

After you have unzipped the archive, you will see a "DRVPCS7_SINA_60" directory on your computer with the block setup. The block is integrated into your PCS7 system when the setup is run (start the "install.bat" file).

Note: The block will be included in Drive ES PCS7, from Version 6.0 Service Pack 1 (planned release for general availability is 03/2004).

DRVPCS7_SINA_60.zip ( 20430 KB )

For additional information, please contact your local Siemens office.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.