Entry type: FAQ Entry ID: 17822789, Entry date: 01/20/1999
(0)
Rate

Video channel extension at IPC RI45 without HIGRAPH II

  • Entry
  • Associated product(s)

QUESTION:
Can the video channel extension still be used in an operation without HIGRAPH II?

ANSWER:
Synchronizing the monitor via the green signal is no longer possible. This is why a
5-way cable with a 15-way/3r subminiature "D" connector <-> 5 x BNC is required
that is available under the order no. 6BK1101-0xy0-0AA0. This cable can be used
for distances of up to 99 m. The dummy xy corresponds to the following length code:
x=A: 10 m, x=B: 20 m ...
y=0: 0 m, y=1: 1 m ...

Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.