×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 18153577, Entry date: 01/20/2004
(0)
Rate

SIMATIC WinCC/ProAgent Version 6.0

  • Entry
  • Associated product(s)

Effective immediately, the WinCC option package SIMATIC WinCC/ProAgent Version 6.0 is released in connection with the following WinAC versions:

  • WinAC RTX V4.0 + SP2
  • WinAC Basis V4.0 + SP1

Product Description

At the time of the release of WinCC/ProAgent V6.0, there were still problems with acknowledging Alarm-S messages in connection with WinAC, if the new message number procedure of STEP7 5.2 was employed (CPU-wide message number band).

These problems have been resolved with the new service packs of WinAC (see above). The retest with WinCC/ProAgent V6.0 could be completed successfully.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.