×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 18475312, Entry date: 09/30/2010
(5)
Rate

How do you connect a 2-wire measuring transducer to analog module 6ES7 331-1KF0.-0AB0, a compact CPU or a C7 device?

  • Entry
  • Associated product(s)

Connecting 2-wire measuring transducers to analog module 6ES7 331-1KF0.-0AB0, a compact CPU or a C7 device
For analog modules that can be configured for 2-wire measuring transducers, please refer to the descriptions in the relevant manuals.

This description covers the following configurations:

  • Analog modules that can only be configured for 4-wire measuring transducers,
    like analog module 6ES7 331-1KF0.-0AB0.
  • Mixed operation of 2-wire and 4-wire measuring transducers on one channel group.
  • Compact CPUs or C7 devices.

Definition of the different transducers:

  • 4-wire measuring transducers have a separate power supply and two measuring cables that are connected to M+ and M- of the analog module. For this reason they are also called active measuring transducers.
  • 2-wire measuring transducers are also called passive measuring transducers, because they are normally supplied via the analog module.

To connect a 2-wire measuring transducer to an analog module (e.g. 6ES7 331-1KF0.-0AB0), a compact CPU or a C7 device, you need an external 24V power supply (Fig. 1).
This supply to the 2-wire measuring transducer must be short-circuit-proof. Provide a fuse to protect the power supply unit (Fig. 1). Please note that the analog input is not protected against destruction in case of a measuring transducer defect (short-circuit). For this case, make sure that you take the appropriate protection measures.


Fig. 1: Connecting 2-wire measuring transducers (block diagram)

M+: Positive measuring circuit
M-:  Negative measuring circuit
MANA: Reference potential of the analog measuring circuit
M :  Ground connection
L+:  DC 24V voltage supply connection

Notes:

  • The marking of the inputs depends on the module type; e.g. M+, M- .
    Please refer to the circuit diagrams for the individual modules.
  • The analog module must be configured in the HW Config as a 4-wire measuring transducer.
    This also applies when operating a mixture of 2-wire and 4-wire measuring transducers on one channel group.
  • Please refer to the description of the relevant module:
    S7-300 Programmable Logic Controller Module Data; Entry ID: 8859629
    CPU 31xC and CPU 31x, Technical Data Device Manual; Entry ID: 12996906
    In the case of C7 devices, separate descriptions have been assigned for each device.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.