Entry type: FAQ, Entry ID: 18752994, Entry date: 11/09/2015

Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC WinCC?

  • Entry
  • Associated product(s)
Microsoft regularly rectifies security gaps in its products and makes these fixes available to its customers in the form of official patches.

These updates/patches are usually issued every second Tuesday in the month, on so-called "Patch Tuesday". Microsoft divides up the updates into numerous different classifications:


However, you only have to install "Security Patches" and "Critical Patches" to ensure that SIMATIC WinCC operation is secure and stable. For this reason, a WinCC test configuration has been set up in order to test the compatibility of the WinCC software with the above-mentioned patch classifications ("Security Patches" and "Critical Patches"). This system always features the very latest of the released versions of WinCC and Microsoft products released for operating these versions of WinCC. Compatibility tests with the latest released versions of WinCC are performed on the test system in pace with the updates published by Microsoft.
We recommend installing all the available updates of both the named classifications to ensure that the system is protected.
Through any additional software installed on your system, it might happen that you have more updates installed than checked by our tests. Of course, nothing can be said about the compatibility of these additional updates. Therefore, we recommend installing all the updates in the separate project-specific test environment prior to rolling out the updates in the productive environment.

In rare cases an update might have a negative effect on our software in our tests. This is noted in the following list in the "Test Result" field. Furthermore, we inform you as fast as possible by newsletter of any indications and the resulting remedies.

Excel file updates with negative influence
Registration required security_patches_failed.xls (12.4 KB)

Recommended procedure for patch management with the Microsoft Windows Server Update Service (WSUS)
These instructions assume that you have a WSUS installed for your WinCC plant. How to proceed with the WSUS is described in Entry ID: 38621083.

1WSUS configuration:
In the "Products and Classifications" dialog you select the "Products" tab and then all the Microsoft products relevant for the plant.
2WSUS configuration:
In the "Products and Classifications" dialog you select the "Classifications" tab and then "Definition Updates", "Security Updates" and "Critical Updates".

Fig. 01

3WSUS configuration:
Create the project-specific groups for distribution of the updates in the plant.
4WSUS administration:
Select all the available updates in the "Critical Updates" and "Security Updates" categories and then deselect the non-released patches as in the list above. Release the patches for installation in the groups created.
5Log in on the clients connected to the WSUS using an administrative account (the clients were configured to receive the updates from the WSUS).
6Execute the updates offered.

You can find more precise information about Industrial Security in connection with WinCC software in the WinCC Security Concept in Entry ID: 60119725.
For more detailed explanations about Microsoft Updates and the WSUS visit the following Microsoft sites.


  • To find out which Microsoft Patches are installed on the PC, refer to Entry ID: 48844294.
  • These guidelines apply only for WinCC V6.0 SP4 and higher.

The procedure described above does not apply for new Microsoft Service Packs which still require an explicit release for use. If the patches require a higher version of the Microsoft software, then refer to the "WinCC Install Notes" or Entry ID 64847781, to check whether these higher versions of the software or Service Packs are released for SIMATIC WinCC.

Additional Keywords
Windows Update Service, Security Patch