×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 18791818, Entry date: 04/08/2004
(0)
Rate

Presetting the maximum number of lines in the WinCC Configuration Tool

  • Entry
  • Associated product(s)

QUESTION:  
How can I preset the maximum number of lines in the WinCC Configuration Tool?

ANSWER:  
The default maximum number of lines set in the WinCC Configuration Tool is 2000.



Fig. 1: Default setting of the maximum number of lines

Proceed as follows to change this value:

Create a new WinCC project folder. Select "No connection".



Fig. 2: Creating a new WinCC project folder

Change the value of the maximum number of lines to the value you require between 1000 and 65535, e.g. 15000.



Fig. 3: Changing the maximum number of lines to the required value

Save the project folder.

Now, when you create a project map, the maximum number of lines is set to the value you have just set in the procedure above.


Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.