Entry type: FAQ, Entry ID: 18924842, Entry date: 05/06/2004
(1)
Rate

Sample Program: S7 Communication with blocks FB14 ("GET") und FB15 ("PUT") of the CPU 317-2PN/DP

  • Entry
  • Associated product(s)

QUESTION:  
How are the loadable communication blocks FB14 ("GET") and FB15 ("PUT") programmed for a data exchange on the S7-300 with a CPU 317-2PN/DP?

ANSWER:  
In order to exchange data between two S7-300 stations with a CPU 317-2PN/DP via a S7 connection which was configured with NetPro, in the S7 program communication blocks must be called. The block FB14 ("GET") serves to retrieve data out of a remote CPU and the block FB15 ("PUT") to write data into a remote CPU.

Properties of the Communication Block FB14 ("GET") and FB15 ("PUT") of the CPU 317-2PN/DP

  • FB14 and FB15 are asynchronous communication functions.
  • The blocks may run through several OB1 cycles.
  • FB14 or FB15 are activated via input parameter REQ.
  • The end of job is indicated by DONE, NDR or ERROR.
  • PUT and GET can communicate simultaneously via a connection.
  • The blocks are contained in a standard library of STEP 7 V5.3.

Attention:
You cannot use communication blocks of library SIMATIC_NET_CP for CPU317-2PN/DP.

The sample program contains a S7 connection via which data can be retrieved with a FB 14 from a remote CPU and data can be written with a FB15 into a remote CPU.

Description of the Sample Program

The STEP 7 project contains two stations S7-300 with CPU 317-2PN/DP for communication via Industrial Ethernet. A S7 connection was setup as the communications basis between both stations. In NetPro, if you open the properties of the S7 connection via "Right mouse click > Object properties", you can view the block parameter "ID" of the communication block. This information has to be taken into account, when calling FB14 or FB15, in order to facilitate a data exchange via a S7 connection.

  Fig. 1: Properties of the S7 Connection ( 53 KB )  

The STEP 7 program consists of blocks OB100, OB1, FB100, DB100, DB200, DB201, FB14 and FB15.

  • OB100
    OB100 is a start up OB and is executed during a reboot of the CPU (warm start). In this OB M1.0 and M0.1 release the first communication trigger.


Fig. 2: OB100 

  • OB1
    OB1 is called cyclically. In this OB the call of the FB100 (instance DB: DB100) is done with M1.0 and M0.1. After FB100 was executed, M1.0 is reset.


Fig. 3: OB1 

  • FB100
    FB100 is called in the OB1 cycle. In this FB you find the call of the FB14 ("GET") and FB15 ("PUT"). FB14 is activated via input parameter "REQ", if the interval marker M10.6 has a positive edge and no job is running.
    The input parameter ID must be adopted from the properties dialog of the S7 connection in NetPro (Fig.1). Parameter ADDR_1 contains that data area that is to be retrieved from a remote CPU. Parameter RD_1 contains the data area for retrieved data. Output parameters NDR, ERROR and STATUS are required for job evaluation and are only valid in the same cycle!


Fig. 4: FB100 - Invoking FB14

If the block was processed with error, the status word of the block is saved for error analysis.


Fig. 5: FB100 - Saving the Status Word

FB15 is activated via input parameter REQ, if clock memory M10.6 has a positive edge and no job is running. Input parameter ID must be adopted from the property dialog in NetPro (Fig.1). In case of parameter ADDR_1 the data area must be stated in the remote CPU, to which the values are to be written. With parameter SD_1 the address of the data to be sent is preset. Output parameters DONE, ERROR and STATUS are required for evaluating the job and are only valid in the same cycle!


Fig. 6: FB100- Invoking FB15

If block was processed with error, the status word of the block is saved for error analysis.


Fig. 7: FB100 - Saving the Status Word

STEP 7 Project as Download:
STEP 7 project contains a sample program on invoking the FB14 and the FB15 with status evaluation. It was designed with STEP 7 V5.3.

Cpu317-2_PUT_GET.exe ( 364 KB )  

Copy file "Cpu317-2_PUT_GET.exe" into a separate directory and then start the file with a double click. The STEP 7 Projekt will be automatically unpacked with all sub directories. You can now open and edit the project with SIMATIC Manager.