×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 19021092, Entry date: 05/28/2004
(0)
Rate

Difference between ALM and SIMATIC Logon

  • Entry
  • Associated product(s)

QUESTION:  
What are the differences between theAutomation License Manager (ALM) and SIMATIC Logon?

ANSWER:  
The Automation License Manager is the tool supplied for STEP 7 V5.3 for managing the License Keys in STEP 7. The use of SIMATIC Logon requires a fee. It provides user administration for both the SIMATIC Software and the License Keys. The following brief description of the functions shows the differences between both programs.

Automation License Manager V1.0

  • Transfer of License Keys to the local hard disc.
  • Transfer of License Keys via network PC (ALM must be installed on the server).

Fig. 1: Settings of ALM V1.0

Automation License Manager V1.1

  • Transfer of License Keys to the local hard disc.
  • Transfer of License Keys to a network PC (ALM must be installed on the server).
  • Use of License Keys on a network PC (ALM must be installed on the server).

Fig. 1: Settings of ALM V1.1

SIMATIC Logon

SIMATIC Logon is a software-package that assigns authorizations for SIMATIC applications and facility areas. It includes following components:

  • SIMATIC Logon Service
    The basis package with central access protection for SIMATIC applications and plant areas.
  • SIMATIC Logon Service STEP 7.
    An option package for embedding SIMATIC Logon Service into the SIMATIC Manager.
  • SIMATIC Logon Admin Tool - permits tasks administration.
    An option package that facilitates the assignment of authorizations (Windows-Groups, function-related rights , ...) for the tasks of an application (SIMATIC BATCH, WinCC, ...). 
    The access protection can be started by logging into the Logon-feature (keyboard), via a chip card-reader or via other devices.

Note:
Using the option packages requires the installation of the basic package. 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit