×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 19078608, Entry date: 07/06/2004
(0)
Rate

SIMATIC WinCC/Dat@Monitor Web Edition V6.0 SP1 available now (SR/DR)

  • Entry
  • Associated product(s)

Effective immediately, the SIMATIC WinCC/Dat@Monitor V6.0 SP1 is available for delivery. Please note that this new version REQUIRES WinCC V6 SP2. A corresponding update from WinCC V6.x to SP2 can be requested via the Internet (article ID 18803944). With the availability of the Dat@Monitor V6.0 SP1, the sale of the SIMATIC WinCC/Dat@Monitor V6.0 will be stopped. The new version cannot be installed on WinCC stations with older version levels (WinCC V6.0 or WinCC V5.x).



1.0 SIMATIC WinCC/Dat@Monitor V6.0 SP1 - What's new?

With Version 6.0 SP1, new functions are introduced. They are:

  • Support for Windows 2003 and Windows 2000 SP4

  • Automatic reconnect in Dat@Symphony

  • Expanded installation options in Windows 2000 networks

  • Support for alarm archives in Dat@Workbook

  • Performance enhancements in Dat@View

In addition, all previously published hotfixes are being consolidated in V6.0 SP1.

1.1 Support for Windows 2003 und Windows 2000 SP4

Starting with the Dat@Monitor V6.0 SP1, the operation under Windows 2003 (Server) and Windows 2000 SP4 (Professional, Server) is released on the server-side as well as the client-side (in addition to the previously released operating systems).

1.2 Automatic Reconnect

Currently, if a Dat@Monitor server fails, the Dat@Symphony clients connected to it are informed about this circumstance, but a reconnection is only possible through repeated manual interaction. Starting with SP1, it can now be specified for each server whether and in what cycle an automatic reconnect should be performed.

1.4 Expanded Installation Options in Windows 2000 Networks

Starting with the Dat@Monitor V6.0 SP1, it is now also possible to install the client components under limited Windows user rights. This is particularly useful for network installation in Windows 2000/2003 domains, in which users are granted only extremely limited rights.

Depending on the selected installation type, the client software can be published for a certain group of users, who can then actively start this installation. As an alternative, the installation of the Dat@Monitor clients can also be specified for certain user logins, which is then automatically executed upon login. System administrators have the ability to configure the installation paths.

1.5 Support for Alarm Archives in Dat@Workbook

Starting with the Dat@Monitor V6.0 SP1, it is now also possible to integrate alarm archive data in Excel reports. In this manner, statistical analyses of alarm states can be employed to - for example - determine the availability and failure behavior of machines/lines/processes. For each alarm archive, the alarm blocks, time ranges and selection criteria to be analyzed can be configured.

1.6 Performance Enhancements in Dat@View

In Dat@View, a number of performance enhancements result in a faster data retrieval. 

When accessing the Dat@View server, it is now also possible to include swapped out database segments located on the server in the analysis.

2.0 Updates and Compatibility to older Dat@Monitor Versions 

Updates from the Dat@Monitor V6.0 to SP1 can be ordered via the download pages of the Customer Support website (article ID: 19064108).

2.1 Dat@Monitor Server
Older Dat@Monitor versions can be upgraded to V6 SP1. In this case, the old Dat@Monitor is first deinstalled and then the Dat@Monitor V6.0 SP1 installed.

2.2 Dat@Monitor Client
The Dat@Monitor server checks the version compatibility between server and client and, if required, automatically installs the corresponding client component. This means:

  • An 'old' Dat@Monitor client V6.0 encounters a current server V6.0 SP1 -> Current Dat@Monitor client V6.0 SP1 is automatically installed
  • A current Dat@Monitor client V6.0 SP1 encounters an 'old' Server V6.0 -> Communication will continue to function, but with the function scope of V6.0

3.0 Installation Requirements

3.1 Hardware Requirements

 

Minimum

Recommended

CPU

DM Client: Intel Pentium II, 300 MHz
DM Server: Intel Pentium III, 800 MHz
Dedicated DM Server: Intel Pentium 4, 2 GHz
Terminal Server: Intel Pentium IV, 2 GHz

DM Client: Intel Pentium III, 300 MHz
DM Server: Intel Pentium 4, 2 GHz
Dedicated DM Server: Intel Pentium 4, 3 GHz
Terminal Server: Intel Pentium 4, 3 GHz (Multi-Processor)

Main Memory (RAM)

DM Client: 128 MB
DM Server: 256 MB
Dedicated DM Server: 512 MB
Terminal Server: 512 MB + 40 MB per Session

DM Client: 256 MB
DM Server: 512 MB
Dedicated DM Server: 1 GB
Terminal Server: 1 GB + 40 MB per Session

Graphics Card

16 MB

32 MB

Color Depth

256

True Color

Resolution

800 x 600

1024 x 768

3.2 Limitation

For the time being, the use of hyperthreading operating modes is not released!

3.3 Software Requirements

  • Dat@Monitor Client:
    • Windows XP Professional with Service Pack 1

    • Windows 2000 Professional with Service Pack 3 or Service Pack 4

    • Windows 2000 Server with Service Pack 3 or Service Pack 4

    • Windows XP Home

    • Windows NT 4.0 SP6a

    • Windows 2000 Server Terminal Services (Win9x, WinCE, Win3.x, ...)

    • Windows 2003 Server Terminal Services (Win9x, WinCE, Win3.x, ...)

    • Internet Explorer 6.0 or higher

    • Excel 2000 or Excel XP (for Dat@Workbook)

  • Dat@Monitor Server:

    • Windows 2000 Professional/Server with Service Pack 3 or Service Pack 4

    • Windows XP Professional with Service Pack 1

    • Windows 2003 Server

    • Internet Explorer 6.0 SP1

    • Microsoft SQL Server 2000 with Service Pack 3 (included in the WinCC product delivery)

    • IIS (comes with Windows)

    • WinCC V6.0 SP2 or Fileserver V6.0 SP2 (on the WinCC V6.0 SP2 CD-ROM)

    • MS Office 2000 SP3 or MS Office XP SP2 (for Dat@Workbook and Dat@View)

For the simultaneous operation of 3 or more Dat@Monitor clients, a server operating system is required on the Dat@Monitor server.

4.0 Delivery Scope and Ordering Data

The delivery of the Dat@Monitor V6.0 SP1 includes two CD-ROMs (Dat@Monitor product CD-ROM und MS SQL Server 2000 SP3 CD-ROM), an authorization disk and the license certificate. The documentation in five languages is contained on CD-ROM. A separate hardcopy (printed) version is not available.

 

Product Name

Order Number

WinCC/Dat@Monitor V6.0 SP1
- Basic Package (3 Client Licenses)
- 10 Client Licenses
- 25 Client Licenses
- 50 Client Licenses


6AV6371-1DN06-0AX1
6AV6371-1DN06-0BX1
6AV6371-1DN06-0CX1
6AV6371-1DN06-0DX1

WinCC/Dat@Monitor V6.0
PowerPacks
- From 3 to 10 Clients
- From 3 to 25 Clients
- From 3 to 50 Clients
- From 10 to 25 Clients
- From 10 to 50 Clients
- From 25 to 50 Clients



6AV6 371-1DN06-0AB0
6AV6 371-1DN06-0AC0
6AV6 371-1DN06-0AD0
6AV6 371-1DN06-0BC0
6AV6 371-1DN06-0BD0
6AV6 371-1DN06-0CD0

The ordering data for WinCC V6.0 SP2 can be found in the corresponding Delivery Release (article ID 18822752).


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.