×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 19164182, Entry date: 07/08/2011
(0)
Rate

Why does it take 3 to 5 minutes for the Login Box to open on the client or until the message "No authorization for operation" is displayed?

  • Entry
  • Associated product(s)

Description
If the Basic Process Control (BPC) package is installed on a WinCC client in the WinCC network, the authorization check is made in a different way to when BPC is not installed. In this case BPC has to be installed on the server, because otherwise querying of the authorizations on the servers does not occur in the expected way and therefore the answer appears only after a certain delay.

Basic Process Control therefore either has to be installed on all the computers (server and clients) in a WinCC project or on none of them.

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.