×
Siemens Industry Online Support
Siemens AG
Тип сообщения: Часто задаваемые вопросы ID сообщения: 19188460, Дата сообщения: 23.02.2016
(4)
Оценить

Which hardware can be connected to the USB port on HMI operator panels?

  • Сообщение
  • Относится к продукту(ам)
Connection of external devices to the USB port of HMI operator panels.

Configuration Note
You can connect the devices listed below to the USB port of HMI operator panels. Which panels have a USB port is shown in Entry ID: 21847868.
 

Device Comments
Standard
USB mouse
-
Standard
USB keyboard
Notes
The operating system of the operator panels does not support German umlaut characters.
Basic Panels 2nd Generation do not have Windows CE.
USB keyboard with trackball or touchpad The following operator panels were tested by way of example with both keyboards.
  • MP277
  • TP177B
  • ThinClient

Note
The operating system of the operator panels does not support German umlaut characters.

USB stick See Entry ID: 21847868.
USB printer See Entry ID: 11376409.
 
Note
Basic Panels 2nd Generation do not support printers.
Mobile hand-held barcode reader for 1D / 2D codes Recommended hand-held barcode readers
  • SIMATIC MV320
  • SIMATIC MV340

Please note that you can only use hand-held barcode readers which convert the barcode internally into an ASCII keyboard code.
 


Fig. 01

 

Note
As far as operator panels are concerned, the hand-held barcode readers operate as keyboards. To read a value into an operator panel, you must put the focus on an input field. To transfer the value directly into the variable of the text field the scan procedure must be terminated with an ENTER (CR).
You enable the ENTER function by scanning the corresponding DMC code in the manual.


A detailed description of the devices is available in the relevant manuals in the following entry IDs.

  • SIMATIC MV320/ SIMATIC MV325 (Entry ID 78905254).
  • SIMATIC MV340 (Entry ID 61909865).
Industrial
USB Hub 4
The Industrial USB Hub 4 primarily serves as USB hub for the connection of peripheral devices to Panels, Multi Panels and Panel PCs with integrated USB port. The simultaneous connection of up to four peripheral devices - such as USB stick, printer, keyboard, mouse, hand-held barcode reader - to one panel is possible with the Industrial USB Hub 4.
 


Fig. 02
 

Remark
More information on the Industrial USB Hub is available in the Catalog ST80 and Entry ID: 23577105.

 
Important

  • The above recommendations do not reflect any official endorsement of equipment - except for the Industrial USB Hub 4. They simply represent a recommendation which is based on previous experience. In other words, responsibility for the use of these devices rests with you.
  • The current carrying capacity of the USB port differs depending on the type of operator panel. Refer to the relevant device manual in each case for precise specifications. It might therefore be necessary to provide an extra power supply for the device connected, for example, via the Industrial USB Hub 4.

Security Notes
Siemens offers products and solutions with industrial security functions which support the secure operation of plants, solutions, machines, devices and/or networks. They are important components in a comprehensive industrial security concept. The Siemens products and solutions continue to be developed under this aspect. Siemens recommends that you keep yourself regularly informed about product updates.
For the safe operation of Siemens products and solutions it is necessary to take appropriate security measures (cell protection concept, for example) and to integrate each component in an overall industrial security concept which is state of the art. This should also cover the third-party products used. Additional information about Industrial Security is available here:
https://www.siemens.com/industrialsecurity.

Additional Keywords
USB devices, Trackball, Barcode scanner, Data Matrix Code, DMC


Указания по безопасности
Для обеспечения и дальнейшего поддержания кибер-безопасности технической инфраструктуры, систем, машин и сетей необходимо внедрить комплексную концепцию информационной безопасности, которая соответствует последним достижениям науки и техники. Продукты и решения Сименс являются всего лишь одним из компонентов такой концепции. Более подробную информацию о кибер-безопасности можно получить здесь
https://www.siemens.com/cybersecurity#Ouraspiration.
Поддержка статистики
Данная функция позволяет выдавать идентификаторы (ID) результата поиска согласно желаемому количеству (формат .txt)

Генерировать список
Копировать URL
Отобразить эту страницу в новом дизайне
Панель управления mySupport
Ссылки по теме